2020-09-21 11:36 PM
Hi
After updating to CubeMx 6.0.1 and my STM32H7 Pack to 1.8.0 I cannot create project code for Keil uVision 5.27.
After pushing the create code button it brings up the progress bar, seems to be doing stuff and then brings up a dialog:
---------------------------------------------------------------------------------------------------------------------------------------
"The code is successfully generated under G:/LoranReceiver_002 but MDK-ARM V5.27 project generation have problem."
---------------------------------------------------------------------------------------------------------------------------------------
When I open uVision I get an error:
--------------------------------------------------------------
"Error: Device not found -
Device: '??device??'
Vendor 'STMicroelectronics'
Please update your device selection."
--------------------------------------------------------------
The uVision file tree is empty of files and when you open the uVision config dialog no device is selected.
I tried the same project with Atollic and it worked fine.
I have not made any changes to uVision 5 since I used it successfully with older versions of CubeMX.
All my MCU packages are up to date in uVision.
I tried ti with an STM32H743ZIT and an STM32F411RE and had the same problem with each.
I have NEVER had any problems with the CubeMX uVision 5.xx before today.
An no I'm not going to change to TrueStudio, it's hard way of doing a simple job and I don't want to waste my time grappling with Eclipse.
Can anybody assist?
Best regards
Rob
2020-10-05 09:46 PM
Hi,
Could you please share your .ioc file? I am not able to replicate your issue.
Regards,
Hugues
2020-10-05 10:41 PM
2020-10-05 10:53 PM
2020-10-06 05:51 PM
2020-10-06 07:18 PM
2020-10-06 07:25 PM
2020-10-06 07:45 PM
Hi,
It's just a random .ioc file I had laying around.
You should be able to upload the .ioc file here.
I don't have direct access to the support case but I've asked someone who does.
Regards,
Hugues
2020-10-06 08:09 PM
2020-10-06 08:44 PM
Hi,
Find attached your .ioc file.
I was able to replicate your issue.
I fixed it by erasing eveything but your .ioc and regenerating the project with CubeMX. Let me know if that works for you.
If it doesn't, please upload your CubeMX logs. These can be found under C:\Users\***\.stm32cubemx\STM32CubeMX.log
Regards,
Hugues