2021-06-01 6:34 AM
Hi!
I cannot change Application Structure from "Basic" to "Advanced".
Same posts (post1, post2 ) did not solve the problem.
Solved! Go to Solution.
2021-06-01 6:50 AM
Hello @Vyacheslav ,
In fact, some project settings options become read-only once the project is saved. To modify these options, the project must be saved as a new project using the File> Save Project as menu:
The Application Structure is one of those options, thus it should be set before the first code generation.
Otherwise, you can re-save the project using Save Project as…
Hope this answers your question. If this this case, please click on the Select as Best button on my reply . This will help other members of the community find this solution more quickly :)
Khouloud.
2021-06-01 6:50 AM
Hello @Vyacheslav ,
In fact, some project settings options become read-only once the project is saved. To modify these options, the project must be saved as a new project using the File> Save Project as menu:
The Application Structure is one of those options, thus it should be set before the first code generation.
Otherwise, you can re-save the project using Save Project as…
Hope this answers your question. If this this case, please click on the Select as Best button on my reply . This will help other members of the community find this solution more quickly :)
Khouloud.
2021-06-01 6:58 AM
Thanks, Khouloud !
This works, but the brain can be broken :)