Skip to main content
FSere.1
Associate
September 16, 2020
Question

Cannot change Application Structure

  • September 16, 2020
  • 5 replies
  • 1750 views

Hello, i cannot change Application Structure to Basic in STM32CubeIDE V 1.4.2

This topic has been closed for replies.

5 replies

Markus GIRDLAND
ST Employee
September 16, 2020

Hello FSere!

If you mean how to switch between flat and hierarchical project structure used for example in dual core projects then it's explained in the devices corresponding application note. For H7 devices, for example, it's explained in chapter 1.3.1 and can be found here: AN5361.

If I misunderstood your question then please provide some additional details about what the problem is and I'll look into it.

FSere.1
FSere.1Author
Associate
September 16, 2020

Hello Markus,

i was meaning the application Structure that is in the project manager in the .ioc file.

0693W000003RpFrQAK.png

Sorry for not being detailed and for my bad english.

Markus GIRDLAND
ST Employee
September 16, 2020

No worries! If it's easier for you then feel free to use another language and I can use google translate and hopefully still understand :smiling_face_with_smiling_eyes:

I'm not as knowledgeable about CubeMX (I'm in the CubeIDE team) but it seems that this is a known bug according to this thread.

It seems that you can use the stand-alone CubeMX tool to select Basic Application Structure and then generate a project for CubeIDE.

FSere.1
FSere.1Author
Associate
September 16, 2020

Ok, i tried with CubeMX and it worked, but when compiling it seems that it cannot see the files under the Drivers directory