Can you have too many peripheral init functions?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-10 3:23 PM
Here is a weird one for ya.
I am programming on the STM32L4R9I-EVAL dev board, but my project is configured
for the STM32L4S9AII6. I am clocked at 120MHz.
My program has started failing for what seems to be because I have too many
MX_<peripheral>_init() functions. Can you configure too many peripherals?
I started getting this bug off and on as I was getting my TIM15 peripheral up and
running. I now have my TIM15 working, or I should say I had it working until
now. I thought before that the TIM15 was the culprit as that was what I was
working on. So I would comment out it's init function in main() and then the
error would go away. I would mess around some more in MxCube and then the
problem would go away (for a while). This seemed to be a repeating theme as I
worked on that.
So I moved on writing a small amount of other code that had nothing to do with any
peripheral and this problem happened again. Only this time, I don't dare mess
with MxCube because before this everything was working perfectly. What is funny
now though is that I notice that the problem goes away when I comment out
MX_TIM15_Init() as before, but now I thought to try commenting out other
peripheral init functions as well. Low and behold, it doesn't matter what init
function I choose to comment out. If I comment out any one of them, this error
goes away.
Enough of the back story, here is the error that I am referring to:
After attempting to run HAL_Init() at the very beginning of the program (and before
any peripheral init function has a chance to be called), the program tries to
run code outside the allocated memory space as shown here:
This is super weird to me because (again) the error occurs before any peripheral init function has a chance to run. So how in the world does commenting out code that never has a chance to execute cause this error to go away? Again, do I have to many peripheral init functions? Again, it does NOT matter which function I choose to comment out, the problem will go away if I comment out ANY one of them.
Here are the init functions as they currently exist in my program:
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_DAC1_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_IWDG_Init();
MX_OCTOSPI1_Init();
MX_OCTOSPI2_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_SPI3_Init();
MX_TIM15_Init();
MX_USART1_UART_Init();
I'm sorry but this is just weird. Any hints would be greatly appreciated. Thanks!
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
-
STM32L4 series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-17 1:30 PM
Those are CPU core registers and are documented in a "programming manual". In this case of Cortex-M4 it's the PM0214.

- « Previous
-
- 1
- 2
- Next »