2019-08-15 7:03 PM
I'm trying to port some firmware from nucleo-F334 to nucleo-G474 for the HRTIM timers and the CubeMX for G474 for HRTIM1 is not working. I found some missing statement in the initialization.
I found that the CubeMX 5.3 initlization code missing a part; specifically the HRTIM clock initialization where the PLL is defined. There's a related constant that also needs to be defined. In any case can someone confirm the problem and how long it may take to get the updated patch.
G474 clock initialization:
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
F334 clock initialization:
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_HRTIM1|RCC_PERIPHCLK_TIM1;
PeriphClkInit.Tim1ClockSelection = RCC_TIM1CLK_PLLCLK;
PeriphClkInit.Hrtim1ClockSelection = RCC_HRTIM1CLK_PLLCLK;
Expand Post
2019-08-17 3:40 PM
I should add that this is only for the HRTIM timers. Would be interested in anyone using the HRTIM timers with G474 and getting success or similar problem; I'm looking into an assembler patch; the other alternative is to continue on the F334 until a bug fix comes through.