cancel
Showing results for 
Search instead for 
Did you mean: 

B-L475-IOT01A+FREERTOS+X-CUBE-BLE1 does not build

CLiu.0
Associate

Hi there,

I am using the latest CubeMX to generate code for B-L475-IOT01A with FREERTOS and X-CUBE-BLE1 4.4.0. However the code it generate does not even build. I tried various samples, including SensorDemoBLESensor, Beacon, but yield the same result.

The build message indicated that MX_BlueNRG_MS_Init() is missing. Apparently it is missing an entire suite of source code. I attempt to port the code over from a Nucleo sample code but was unsuccessful.

Please kindly help to fix. Thanks!

2 REPLIES 2
Karl Yamashita
Lead II

Yeah I've complained about the same issue over a year ago with support. I too can't get it to compile without so many errors. I still haven't seen ST fix the compile errors since then.

I Can't Believe It's Not Butter. If you find my answers useful, click the accept button so that way others can see the solution.
DGarc.5
Associate II

Any answer?