2023-10-09 03:45 PM
Trying to download Algobuild for CubeMx for Mac. The software package selector says it needs to be downloaded. There is a yellow triangle with an exclamation next to the word "Download". Clicking it does nothing and no explanation what the yellow triangle means.
I tried to download the algobuild package from the ST.com website but it keeps trying to load in a windows environment and I can't see a method to import into the Mac CubeMX. There is a local directory file structure to import but again it is only showing my virtual machine windows directory structure and not the Mac environment.
2023-10-10 02:02 AM - edited 2023-10-10 02:04 AM
Hello @Davidcs,
First let me thank you for posting and welcome to the ST Community.
Can you provide please the STM32CubeMx version which you are using.
Thanks.
Mahmoud.
2023-10-10 06:13 AM
CubeMx version 17.0.6 (10)
CubeIdE version 1.13.2
2023-10-27 09:10 AM
Hello @Davidcs,
Let me thank you for posting.
The download and the install are done successfully on MacOS (CubeMx 6.9.2).
Thanks.
Mahmoud