cancel
Showing results for 
Search instead for 
Did you mean: 

Algobuild software package not downloading in CubeMX for Mac

Davidcs
Associate

Trying to download Algobuild for CubeMx for Mac. The software package selector says it needs to be downloaded. There is a yellow triangle with an exclamation next to the word "Download". Clicking it does nothing and no explanation what the yellow triangle means.

 

I tried to download the algobuild package from the ST.com website but it keeps trying to load in a windows environment and I can't see a method to import into the Mac CubeMX. There is a local directory file structure to import but again it is only showing my virtual machine windows directory structure and not the Mac environment.

3 REPLIES 3
Mahmoud Ben Romdhane
ST Employee

Hello @Davidcs,

First let me thank you for posting and welcome to the ST Community.

Can you provide please the STM32CubeMx version which you are using.

Thanks.

Mahmoud.

CubeMx version 17.0.6 (10)

CubeIdE version 1.13.2

Hello @Davidcs,

Let me thank you for posting.

The download and the install are done successfully on MacOS (CubeMx  6.9.2).

MahmoudBenRomdhane_0-1698422804413.png

Thanks.

Mahmoud