2018-04-22 11:09 AM
Hello!
After upgrading CubeMX to version 4.25In the * .bin code, did the path to the project come up?This is normal?#what-has-changed-in-cubemx-4.25 #what-has-changed-in-cubemx-4.25-from-cubemx-4.172018-05-03 7:24 AM
Hi
Ctef.Oleg
It is normal, this the output of your compiler and it is not related to MX generated project
2018-05-03 10:26 AM
Thank you!
but if I put version 4.17I do not have this lineIt is enough to assemble a simple project without writing a single line of code2018-05-04 3:29 AM
could you attach the ioc please?