cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 Nucleo Pushbutton RTC Conflict

vicsimdelay1
Associate II

Hello,

I've discovered the following anomalous behavior when attempting to use the STM32F103 Nucleo board:

Pushbutton interrupt code will not execute if the RTC is active with NVIC EXTI13.  I've noticed that the RTC tamper PIN is also assigned to PC13 but I've made sure that the output selection is disabled and RTC tamper is deselected inside CudeIDE/CubeMX window.  If the RTC is activated with NVIC EXTI13, I measure zero volts across the appropriate pushbutton (pushbutton not depressed) pins (without the RTC activated the voltage across the same pins is 3.3V). My initial GUESS is PC13 is being reconfigured as an open drain output and being pulled low when the MX_RTC_Init is executed? I've tried to use the debugger to read the appropriate register and bit but I keep receiving a read error.  If I comment out the MX_RTC_Init function and download the program I receive correct functionality from the pushbutton but only after a computer reboot.

I've also tried to execute the MX_GPIO_Init both before and after MX_RTC_Init but the problem still persists.  Is there something inside the generated CubeMX/CubeIDE RTC code that forces PC13 into a different mode? 

I don't have the appropriate tools to attempt my proposed hardware fix which would be to reroute the pushbutton to PB13 and change the configuration and code to match.

 

1 ACCEPTED SOLUTION

Accepted Solutions
vicsimdelay1
Associate II

I found the problem but it seems the CubeIDE/CubeMX setup is confusing at best.

If you activate the RTC and have the Pushbutton interrupt selected you must select NO RTC OUTPUT as RTC OUT under the parameter settings tab for the RTC.  The default is DISABLE when you activate the RTC.  It seems to me that if the pushbutton interrupt is selected to be active that the RTC OUT should default to NO RTC OUTPUT instead of Disable in the ioc screen. In order to lessen the confusion, shouldn't the DISABLE be relabeled as ALARM on the CubeMX screen so the code below would be more similar?

 

Summary:

hrtc.Init.Ouput = RTC_OUTPUTSOURCE_ALARM (is default when RTC OUT ------ DISABLE in ioc screen)

and pushbutton interrupt does not work.

 

once

hrtc.Init.Output = RTC_OUTPUTSOURCE_NONE (which is not default when activating RTC OUT ---- No RTC Output selected) 

the pushbutton is rightfully assigned to PC13 and works.

View solution in original post

6 REPLIES 6
Ghofrane GSOURI
ST Employee

Hello @vicsimdelay1 

First let me thank you for posting.

I'm currently checking this , I will get back to you asap.

I would appreciate it  if you could share your IOC.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Here is one of the ioc files.

Hello @vicsimdelay1 

By checking the generated code using CubeMX  , The function MX_RTC_Init does not contain any code that explicitly configures GPIO pins, including PC13. there is no indication that MX_RTC_Init  directly affects PC13.

 

static void MX_RTC_Init(void)
{

  /* USER CODE BEGIN RTC_Init 0 */

  /* USER CODE END RTC_Init 0 */

  RTC_TimeTypeDef sTime = {0};
  RTC_DateTypeDef DateToUpdate = {0};

  /* USER CODE BEGIN RTC_Init 1 */

  /* USER CODE END RTC_Init 1 */

  /** Initialize RTC Only
  */
  hrtc.Instance = RTC;
  hrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND;
  hrtc.Init.OutPut = RTC_OUTPUTSOURCE_ALARM;
  if (HAL_RTC_Init(&hrtc) != HAL_OK)
  {
    Error_Handler();
  }

  /* USER CODE BEGIN Check_RTC_BKUP */

  /* USER CODE END Check_RTC_BKUP */

  /** Initialize RTC and set the Time and Date
  */
  sTime.Hours = 0x0;
  sTime.Minutes = 0x0;
  sTime.Seconds = 0x0;

  if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }
  DateToUpdate.WeekDay = RTC_WEEKDAY_MONDAY;
  DateToUpdate.Month = RTC_MONTH_JANUARY;
  DateToUpdate.Date = 0x1;
  DateToUpdate.Year = 0x0;

  if (HAL_RTC_SetDate(&hrtc, &DateToUpdate, RTC_FORMAT_BCD) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN RTC_Init 2 */

  /* USER CODE END RTC_Init 2 */

}

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

What about inside HAL_RTC_Init() on line 20?

Updated post.....  It still does not work.  Could use further assistance.

vicsimdelay1
Associate II

I found the problem but it seems the CubeIDE/CubeMX setup is confusing at best.

If you activate the RTC and have the Pushbutton interrupt selected you must select NO RTC OUTPUT as RTC OUT under the parameter settings tab for the RTC.  The default is DISABLE when you activate the RTC.  It seems to me that if the pushbutton interrupt is selected to be active that the RTC OUT should default to NO RTC OUTPUT instead of Disable in the ioc screen. In order to lessen the confusion, shouldn't the DISABLE be relabeled as ALARM on the CubeMX screen so the code below would be more similar?

 

Summary:

hrtc.Init.Ouput = RTC_OUTPUTSOURCE_ALARM (is default when RTC OUT ------ DISABLE in ioc screen)

and pushbutton interrupt does not work.

 

once

hrtc.Init.Output = RTC_OUTPUTSOURCE_NONE (which is not default when activating RTC OUT ---- No RTC Output selected) 

the pushbutton is rightfully assigned to PC13 and works.