cancel
Showing results for 
Search instead for 
Did you mean: 

The updated graphical interface makes me very uncomfortable.

Today, after updating the latest IDE, my interface has changed to this look (Figure 1), which makes me very uncomfortable. How can I change it to the previous look (Figure 2)?be07801a-3f34-4100-8f85-34dbe62b3f93.png旧版.png

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @叱咤月海鱼鱼猫 and welcome to the ST Community.

This is a known limitation, after updating the STM32CubeIDE from some versions to the patch 1.18.1 using the update site updater, the GUI of the integrated STM32CubeFinder and STM32CubeMX are the images of the old UI tools. The workaround is to uninstall and reinstall the STM32CubeIDE directly from the installer on st.com.

It is already reported and added to the STM32CubeIDE:STM32CubeIDE errata 1.18.x - stm32mcu.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Andrew Neil
Super User

That looks unchanged from v1.13.0 - what's the problem?

AndrewNeil_0-1744910870145.png

 

If you're looking for the C editor view, click here - as before:

AndrewNeil_1-1744910954513.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
STTwo-32
ST Employee

Hello @叱咤月海鱼鱼猫 and welcome to the ST Community.

This is a known limitation, after updating the STM32CubeIDE from some versions to the patch 1.18.1 using the update site updater, the GUI of the integrated STM32CubeFinder and STM32CubeMX are the images of the old UI tools. The workaround is to uninstall and reinstall the STM32CubeIDE directly from the installer on st.com.

It is already reported and added to the STM32CubeIDE:STM32CubeIDE errata 1.18.x - stm32mcu.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

AScha.3
Super User

This is , what i got after update 1.18.0 -> 1.18.1 on Linux (MxLinux, up to date):

AScha3_0-1744912296878.png

looking ok - or not ?

If you feel a post has answered your question, please click "Accept as Solution".