cancel
Showing results for 
Search instead for 
Did you mean: 

The monitored data with "spike"

yang2
Associate III

Dear Sir,

When I monitor the data, sometimes the value often accompanied by spikes, such as followed figure.

yang2_1-1728383267255.png

 

In my case, I monitor 3 variables that update from ADC registers.

yang2_7-1728384270751.pngyang2_8-1728384290569.png

Normally, their values would be around 0.

The signals of ADCvalue[0] and ADC Value[1] appear to be normal.

yang2_2-1728383529394.pngyang2_3-1728383540988.png

However ADCValue[2] has some spikes.

yang2_1-1728383267255.png

 

When I verify the variables byIDE, the variable does not show these spikes. It always remains around 0.

yang2_4-1728384076630.png

And I also used a conditional statement to check: if the value is greater than 50 (the maximum spike value is around 260), a counter would increment. However, the counter has always remained at 0, so I believe the actual variable does not have these spikes.

yang2_5-1728384188082.pngyang2_6-1728384212024.png

 

What could be the possible reasons for this?

Best Regards,

 

 

 

 

 

 

 

 

5 REPLIES 5
yang2
Associate III

Additionally, if I add monitoring of other values, there is a chance that the data will return to normal.

yang2_1-1728385808947.png

For example, as shown in the image, I added two more monitoring variables, offset[0] and offset[1].

At this point, ADCvalue[2] returned to normal.

 

TDK
Guru

The spikes are about 256 off of the real value. It's a int16_t value which is sometimes positive, sometimes negative.

I would guess that whatever is reading the value is doing so one byte at a time rather than both bytes at once, which causes the issue. For example, if you read the first byte when the value is -1, and the second byte when it changes to 1, the reading will be around -256.

How to fix? Not sure. Perhaps change the acquisition mode or add a trigger such that it doesn't probe the value when they're being updated.

If you feel a post has answered your question, please click "Accept as Solution".
Billy OWEN
ST Employee

Hi @yang2 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

yang2
Associate III

Hello TDK, 

I think what you said makes a lot of sense. It might really be caused by the fact that it's transmitted as two separate bytes. Thank you for sharing your opinion.

KhPaul
Associate III

I have the same issue and it's really anoing, when you are monitoring low range signals