STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! Bug in STM32CubeMonitor-UCPD log - RDO decoding

Hi,STM32CubeMonitor-UCPD sometimes displays RDOs like this:Where does the number MaximumOperatingCurrent come form? Since the RDO is defined as: typedef struct { uint32_t MaxOperatingCurrent10mAunits : /*!< Corresponding to min if GiveBackFlag = 1 */...

Erlkoenig_0-1715532579913.png

Resolved! How to reset the time in saved log file?

Hallo, I am saving the log files of the chart in the CUBEMonitor software. I read certain values from the MCU through Cube Monitor and save them as .CSV. However I've noticed that the first file I save after opening the software does start from 0 sec...

draco by Associate II
  • 2090 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeMonitor - Trigger SW Reset

Hello,I would like to trigger a STM32 device reset from inside STM32CubeMonitor.I'm developing an application using STM32CubeIDE and STM32CubeMonitor. Duringe measuring of my variables via STM32CubeMonitor it is possible that my device gets into a re...

MKori.1 by Associate III
  • 3800 Views
  • 6 replies
  • 3 kudos

STM32CubeMonitor-RF V2.16.0 is available

Hello A new 2.16.0 version of STM32CubeMonitor-RF is available on st.com. You can download it on https://www.st.com/en/development-tools/stm32cubemonrf.htmlClick on "Get latest" to download the version 2.16.0. What are the main changes in this versio...

Release of STM32CubeMonitor-UCPD 1.4.0

Dear all, We are pleased to announce that STM32CubeMonitor-UCPD 1.4.0 has been released and is available on st.com. This tool is the perfect companion for customers dealing with our USB Type C solution. This new release of STM32CubeMonitor-UCPD suppo...

PDEFO1_0-1732005370092.png
PDEFO.1 by ST Employee
  • 1229 Views
  • 0 replies
  • 2 kudos

Why does CubeMonitor not show variable values?

Hi everyoneI have a - for sure very basic - CubeMonitor flow. The goal later is to achieve a step response for regulator parameter estimating, but at first I want to start with showing temperatures only and fail here. What I managed to do already:Pro...

White_Fox by Associate III
  • 4487 Views
  • 3 replies
  • 1 kudos

Resolved! STM32CubeMonUCPD ibus monitor show value zero

Hello,I am using STM32-U585I-IOT02A board. I have initialized USB-C SINK TCPP project with fixed 9V settings. On STM32CubeMonUCPD, 'ibus(mA)' value is always zero when connected BMS board shows charging current more than 1A. Please let me know if I m...

image.png
Robert7 by Associate III
  • 4247 Views
  • 4 replies
  • 4 kudos