STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Parsing data problem

I'm currently facing a frustrating problem with STM32Monitor. When I'm trying to parse data, the progress bar gets stuck at 10%. As a result, I'm unable to pull the project data list.Hardware environment: Windows 11

85be9243b5d3c717910d6c329e9771d.png

Resolved! STM32WB05KZ monitor

Hello,i use STM32WB05KZ for the bluetooth.With software can use to programme or to do some BLE test ?thanks

ljm by Associate III
  • 1511 Views
  • 3 replies
  • 1 kudos

Resolved! LPM01A cannot connect to STM32CubeMonitor-Power

I downloaded Cube Power Monitor and am trying to use it to connect to the LPM01A. I have downloaded and installed the W8 version of the virtual com port driver. I can select the board in the drop down menu, but when I hit "Take Control", a dialog box...

ADing.1 by Associate II
  • 8659 Views
  • 11 replies
  • 3 kudos

Resolved! USB Driver for power monitor.

Hi  I have the cube monitor plugged in , and running the cube monitor power application. I had it working on my old computer (Windows 10) , but had to install the USB driver of ST web site. Since moving to my new computer, I cant find the driver agai...

STM32CubeMonitor-RF V2.17.0 is available

Hello A new 2.17.0 version of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.17.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.22.0Alignment with STM32CubeWBA firmware...

STM32CubeMonitor 1.10.0 is available

Hello A new version 1.10.0 of STM32CubeMonitor is available on st.com. You can download it on https://www.st.com/en/development-tools/stm32cubemonitor.html Click on "Get latest" to download the version 1.10.0. What are the changes in this version ? N...

Accessing UCPD monitor via USB to UART bridge

Hello,I would like to ask a question, if it is possible to access UCPD monitor via USB-UART bridge? I am following tutorial AN5418, with nucleo G0B1RE and SNK1M1 shield. Everything works fine when I use st-link, but when using uart bridge I dont see ...

Marosh_2-1739441857181.png
Marosh by Associate III
  • 1295 Views
  • 2 replies
  • 0 kudos

The monitored data with "spike"

Dear Sir,When I monitor the data, sometimes the value often accompanied by spikes, such as followed figure. In my case, I monitor 3 variables that update from ADC registers.Normally, their values would be around 0.The signals of ADCvalue[0] and ADC V...

yang2_1-1728383267255.png yang2_7-1728384270751.png yang2_8-1728384290569.png yang2_2-1728383529394.png
yang2 by Associate III
  • 3101 Views
  • 6 replies
  • 1 kudos