STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Acquisition frequency

Hi,I have read (STL32CubeMonitorWiki)  how to opitmize the speed acquisition.As a conclusion, it is written that we can reach 1 000Hz for a single variable. Dumb question: is it the maximum or could it still be improved ?I'd like to reach 40 000Hz (w...

JGreg.2 by Associate III
  • 1513 Views
  • 1 replies
  • 0 kudos

Resolved! Stm32 cube monitor show value zero

I am using STM32H503RB nucleoboard. I have initialized project from cubeMX with default settings and only added a variable 'x' which is incremented with 100ms period. On CubeMonitor, 'x' variable value is always zero. When I debug I can see variable ...

bepot by Associate II
  • 2772 Views
  • 2 replies
  • 1 kudos

Resolved! CubeMonitor frequently Disconnects

The cube monitor frequently disconnects while capturing data. How do i solve this problem i want to log data continuously. The other problem is when i am saving the data as belowi do not know the location where the csv file is stored. Please help.

SRedd5_0-1695829037054.png
SRedd.5 by Senior III
  • 4277 Views
  • 8 replies
  • 1 kudos

Resolved! The exe-config node can't extract variable from elf file

Hello, I followed the tutorial with just one variable (extracted from an elf) there was no problem the variable showed in the chart. But when I added another variable to the code and got a new elf. I went to the variable node to add the new variable ...

NChan.7 by Associate
  • 2175 Views
  • 2 replies
  • 0 kudos

Resolved! Booleans not showing up if C++ "bool" is used

Hello again, I know i posted some time ago but my question is not seen anymore (link to original https://community.st.com/s/question/0D53W00000wWDX2SAO/cubemonitor-still-not-seeing-boolean-values)I was suggested to to include "stdbool.h" but, as I'm ...

MFran.4 by Senior
  • 6149 Views
  • 6 replies
  • 1 kudos