STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

STM32CubeMonitor V1.8.0 is available

Hello A new version 1.8.0 of STM32CubeMonitor is available on st.com. You can download it on https://www.st.com/en/development-tools/stm32cubemonitor.html Click on "Get latest" to download the version 1.8.0. What are the changes in this version ? Sup...

STM32CubeMonitor-RF v2.14.0 is available

Hello A new 2.14.0 version of STM32CubeMonitor-RF is available on st.com. You can download it on https://www.st.com/en/development-tools/stm32cubemonrf.htmlClick on "Get latest" to download the version 2.14.0. What are the main changes in this versio...

STM32CubeMonitor-Power issue/enhancements

The STLink V3-PWR has the potential to be a great tool.  However, STM32CubeMonitor-Power (v1.2.1) has a critical issue that seems likely to generate many unnecessary support calls to ST: there is no way to run the tool without logging acquisitions to...

DAlbe.3 by Senior II
  • 5616 Views
  • 7 replies
  • 3 kudos

IOC configuration for digital signals to go low

Please find the given DSO image !!!! blue is fault signal and yellow is PWM   I need to stop the PWM, if a fault will come, while doing this my PWM is  turning off  but not fully its showing a ramp down of 88usec and then becoming zero. given configu...

IMG_20240306_102611636_HDR (1).jpg
Sushmita by Associate II
  • 1397 Views
  • 1 replies
  • 0 kudos

Resolved! STLink-V3PWR redNode

HiIs there a RedNode plugin / Script for the power measurement with the STLink V3PWR? Or do I need to do that by myself with the UM2269 manual? Thanks in advancenobody

nobody by Associate II
  • 1158 Views
  • 1 replies
  • 0 kudos

Stm32 Cube monitor power having multiple bugs

HiOn windows:1. STLINKv3PWR is not recognised by cube monitor power when connected a USB hub (select Board is empty).2. some times the PC software takes up to 20 seconds to find the comport.3. diconnection of the device (USB) duing acquisition leads ...

MK..1 by Senior
  • 1964 Views
  • 2 replies
  • 0 kudos

v1.8.0 release anytime soon?

Is there a scheduled release date for 1.8.0?Will 1.8.0 include improvements to the elf parser to support non-trivial data structures (i.e., nested structures with arrays, etc.)?

STM Studio Snapshot Acquisition Mode

All,I am trying to use the snapshot acquisition mode in STM Studio to observe variables at user-defined timings, but stuck at setting "the Address of snapshot trace header part."As indicated by the STM Studio manual, I have identified the address of ...

skyy by Associate
  • 1547 Views
  • 1 replies
  • 0 kudos

STM32CubeMonitor-Power Feature Request

Hello,the STM32CubeMonitor-Power is a very useful tool and I am using it a lot.For power optimizing applications often the period, at which current pulses occur, help a lot to find the source. Therefore I am missing a "Cursor" feature for this tool.W...

c_dev05 by Associate III
  • 1641 Views
  • 2 replies
  • 3 kudos