cancel
Showing results for 
Search instead for 
Did you mean: 

New bare metal project STM32MP13 using STM32Cube_FW_MP13_V1.0.0

ravo
Senior

Dears

I would like to create new project from STM32Cube_FW_MP13_V1.0.0 - based on template "BSP_BasicTemplates"

I verified Properties for this project under "Paths and Symbols" - Includes, Libraries, Source ... all looks normal as another project from Application subfolder

But compilation stop on error

 

make -j12 all

make: *** No rule to make target 'C:/Users/Drivers/CMSIS/Device/ST/STM32MP13xx/Source/Templates/gcc/startup_stm32mp135c_ca7.c', needed by 'Example/STM32CubeIDE/startup_stm32mp135c_ca7.o'. Stop.

"make -j12 all" terminated with exit code 2. Build might be incomplete.

Where could be problem ? I hope that templates should have all properly configured...

 

Best Regards

Radim

12 REPLIES 12
ravo
Senior

Dear @DBELL.1 

Do you have any update, will be corrected in next release ?

Radim

Hello @ravo ,

 

Unfortunately, I got no news for this subject.
I sent a reminder to the development team.

rgds,
David 

DBELL.1
ST Employee

Hello @ravo ,

 

FYI, the feature will not be corrected in the next release.

This implies to duplicate too many files and the HAL+FW will become huge in size.

 

rgds,
David B.