Hello,I'm using the Ux_Device_HID_A7 application and I have no probleme with:memory = _ux_utility_memory_allocate(UX_NO_ALIGN, UX_REGULAR_MEMORY, sizeof(UX_SLAVE_CLASS) * UX_MAX_SLAVE_CLASS_DRIVER);
the buffer is properly set at the right address i...
Hello @Stnoobs ,
1. right due to the absence of HAL_XSPI_MODULE_ENABLED2. correct3. I got these ones, but i don't have it while using USART1, and the MX_USART1_UART_Init() is empty4. correct
So, for me, the main issue with QUADSPI is the missing o...
Hello @SL1 ,
I don't have the issue you described with the UX_Device_CDC_ACM.
And I don't see neither the vectors table like you wrote it.Did you make this example with cubeMX or did you use it like it is provided?
rgds,David B.
Hello @zhuij.1
In order to make the FW run in DDR, you have also to remove "monitor reset" in the debug configuration of the "UART_Receive_Transmit_Console_A7", in the startup tab.
rgds,David B.