cancel
Showing results for 
Search instead for 
Did you mean: 

location of target/stm32mp1x.cfg on Windows

Steffen Rose
Associate III

I want to use the STM32CubeIDE to debug the M4 on the STM32MP1.

I setup the debug setting for debug probe ST-Link (OpenOCD). If I use the automated generation of the script, it refer to [find target/stm32mp1x.cfg].

This is not part of the default installation of STM32CubeIDE 1.6.1 and it is not located in

https://github.com/STMicroelectronics/OpenOCD/tree/openocd-cubeide-r3/tcl/target

In general it doesn't seems to be the MP1 openocd files for the MP1 within the windows installation.

2 REPLIES 2
OlivierK
ST Employee

Hi Steffen Rose (Community Member),

 [find target/stm32mp1x.cfg] called from the project debug script is indeed part of the installation of STM32CubeIDE1.6.1

<CubeIDE Install dir>\plugins\com.st.stm32cube.ide.mpu.debug.openocd_xx\resources\openocd\st_scripts\target

Did you install the IDE from this repository?

https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-ides/stm32cubeide.html

Regards,

Olivier

Yes, I did install the official release from ST.

But thank you for your path. It seems my mistake was, that I searched in the *mcu* and not in the *mpu* path of openocd.

I'm unsure, why the user script this not do automatically. But it help's me.

Thank you

Regards

Steffen