User Activity

I work on Win10. DFU is seen in the settings. I use the programmer to transfer the linux image to the customer MP1 board. The transfer is very instable and break on different files/positions. Very seldom the complete *.tsv image is transfered and I c...
I want to use the STM32CubeIDE to debug the M4 on the STM32MP1.I setup the debug setting for debug probe ST-Link (OpenOCD). If I use the automated generation of the script, it refer to [find target/stm32mp1x.cfg].This is not part of the default insta...
I work on Windows and use the STM32CubeIDE 1.6.1. I want to program and debug the M4 part, On the A7 part Linux is working.My current state is, that The A7 is in Bootloader mode and the DFU per USB is connected and shown in Windows (Gerätemanager) a...
Has the MSI with LSE auto calibration a sufficient precision for the 1Mbit CAN bitrate?What is the accuracy compared with a crystal PLL clock?
Posted on March 15, 2018 at 11:41I implemented an error handling after an ECC related NMI is called (double bit error). How can I test it?Typical I overflash with corrupt data. But in case of the STM32L4 the hardware prevent it.Do you know a diffent...
Kudos from