STM32CubeIDE (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 1.16.0 released

STM32CubeIDE 1.16.0 was released today on st.com as well as an in-tool update patch. What is new in 1.16.0?Microcontroller and board lists aligned with STM32CubeMX v6.12.0 : STM32C0 ,STM32WB0 and STM32MP25XXAdded CMake support for multicontext projec...

Resolved! DDR_Init_A7 unable run

DearsI can only start this example in Debug mode, the BLUE led start blinking... So it works OK.But If I try to use RUN command (using icon, or right mouse click on project file) than it seems not work (RED leds blinks only ONE and is OFF, Blue LED i...

ravo by Senior
  • 625 Views
  • 4 replies
  • 1 kudos

Resolved! STM32MP13 empty STM32Cube project "hello world"

HelloCan I use Windows and STM32CubeIDE to develop application using STM32MP135FAF7 (STM32MP135F-DK discovery kit).I tried to create empty project based on this discovery kit but it ended with message"This project requires OpenSTLinux version 'openst...

ravo by Senior
  • 1125 Views
  • 6 replies
  • 2 kudos

STM32CubeIDE 1.14.1 released

Hello, Since the STM32CubeIDE 1.14.0 release, some issues was faced when executing shell script in the pre/post build command. This issue was faced with the Windows version of the STM32CubeDE 1.14.0. Therefore, a patch is now available on ST site whi...

How to enable drivers in kernel using STM32CubeIDE

Is there any way to enable and disable drivers in the kernel from STM32CubeIDE? For example to enable support for another LCD panel If I use menuconfig to change configuration, make does not work anymore.+ case "$command" in + exec make -j12 all *** ...

pj_stm by Associate III
  • 894 Views
  • 5 replies
  • 0 kudos

Resolved! Where is eclipse.ini located

Hi Guys. I want to increase memory allocated to the eclipse, but I cant find the eclipse.ini fille. Could you direct me into a right direction?

pj_stm by Associate III
  • 843 Views
  • 2 replies
  • 0 kudos