2024-03-20 05:13 AM
Hello all,
I have updated the STM32Cube IDE version to the 1.15.0, it has own STLinkUpgrade tool which is also updated to version 3.14.5. But a problem arised. It wants me to update my STLink V2 firmware. When I tried, It gives error like:
"Unexpected flash size for ST-Link Micro. Don`t know how to upgrade."
But I can use the older version 3.13.4 without any problem:
Is there a problem caused by 3.13.5 or caused by my ST-Link V2?
Solved! Go to Solution.
2024-03-27 02:11 AM
Tati_rn, try https://www.st.com/en/development-tools/stsw-link007.html as in my post above, it will do the update to the latest version and stop the warnings for STMCubeIDE.
2024-03-28 06:02 AM
Hello @PHolt.1 ,
Could you please specify the board that you are using?
Otherwise, here are some steps you can take to fix the problem:
Under Window --> Preferences--> Network Connections, activate Native provider
Under Window --> Preferences--> Firmware Updater, click on Check Connection
don't forget Apply and Close, if the connection works.
If that doesn't work, try this:
Hope this helps!
Regards,
Rim.
2024-03-28 08:11 AM
It is a custom design of mine; not an ST board.
The STLINK V3 ISOL firmware update worked. The issue was with Cube IDE reported a missing file (see my post on eevblog; could not post the link here sine this forum removes certain words) but the file was not missing. Multiple threads here too.
I reverted to 1.14.1 and everything works again. I will freeze this project on 1.14.1 because one cannot just keep updating for ever, and allocate time to a production product to sort out a broken new tool version.
2024-03-30 07:31 AM
Thanks to everyone who has tried to solve this problem, but after about 3 hours of messing around, my solution was the same as PHolt.1, revert to 1.14.1.
2024-04-18 03:54 AM
Summary: I tried with the latest ST-LINK Updater exe version 3.15.6 and my problem has been resolved.
Document: Firmware upgrade for ST-LINK, ST-LINK/V2, ST-LINK/V2-1 and STLINK‑V3 boards - Release note
It is happy to see my issue on fixes issues list.
The newer version of updater is not embedded on IDE yet. You need to download from here: STSW-LINK007 - ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 boards firmware upgrade - STMicroelectronics
2024-05-17 03:34 AM
How can I log in to my.st account on stm32cubeIDME, it always reports problems with network devices, saying the module is disconnected, while everything is normal. Can someone help me? Thank