2021-06-28 10:46 AM
I am using STM32CubeIDE v1.6.1 and am seeing some strangeness.
When I call strcat(), I get a hardfault if the end of the string (where the nul is) being catted to is at an odd address?
Here is code from the .list file:
char s1[20];
strcpy(s1, "--");
800ab50: f107 030c add.w r3, r7, #12
800ab54: 4a65 ldr r2, [pc, #404] ; (800acec <sd_cmdproc_process_packet+0x374>)
800ab56: 6812 ldr r2, [r2, #0]
800ab58: 4611 mov r1, r2
800ab5a: 8019 strh r1, [r3, #0]
800ab5c: 3302 adds r3, #2
800ab5e: 0c12 lsrs r2, r2, #16
800ab60: 701a strb r2, [r3, #0]
strcat(s1, "1");
800ab62: f107 030c add.w r3, r7, #12
800ab66: 4618 mov r0, r3
800ab68: f7f5 fbc4 bl 80002f4 <strlen>
800ab6c: 4603 mov r3, r0
800ab6e: 461a mov r2, r3
800ab70: f107 030c add.w r3, r7, #12
800ab74: 4413 add r3, r2
800ab76: 495e ldr r1, [pc, #376] ; (800acf0 <sd_cmdproc_process_packet+0x378>)
800ab78: 461a mov r2, r3
800ab7a: 460b mov r3, r1
800ab7c: 881b ldrh r3, [r3, #0]
800ab7e: 8013 strh r3, [r2, #0]
strcat(s1, "2");
800ab80: f107 030c add.w r3, r7, #12
800ab84: 4618 mov r0, r3
800ab86: f7f5 fbb5 bl 80002f4 <strlen>
800ab8a: 4603 mov r3, r0
800ab8c: 461a mov r2, r3
800ab8e: f107 030c add.w r3, r7, #12
800ab92: 4413 add r3, r2
800ab94: 4957 ldr r1, [pc, #348] ; (800acf4 <sd_cmdproc_process_packet+0x37c>)
800ab96: 461a mov r2, r3
800ab98: 460b mov r3, r1
800ab9a: 881b ldrh r3, [r3, #0]
800ab9c: 8013 strh r3, [r2, #0]
800ab9e: e1c4 b.n 800af2a <sd_cmdproc_process_packet+0x5b2>
}
the strcat of "1" works, but the strcat of "2" hard faults. I suspect it isalignment error with the "strh".
It is also curious that the calls to strcat() (and strcpy()) do not call the actual functions.
I appologize if I have missed something obvious.
Thanks,
mark
2021-06-28 11:22 AM
Are you using a Cortex-M0(+) processor?
Sometimes these calls are folded inline or use intrinsics.
Most Cortex can handle unaligned 16 or 32-bit access, all will fail with LDRD/STRD
Optimization
Correct Core Selection for compiler/libraries
2021-06-28 11:28 AM
Guess I should have included that information at the start...
This project is using a Cortex-M7 (STM32F769NIHx) on the STM32F769I-DISCO board.
Here are the gcc options shown in Properties->C/C++ Build->Settings->MCU GCC Compiler->All Options:
-mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F769xx -c -I../Core/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/CMSIS/Include -I"C:\Users\mbutsch\STM32CubeIDE\workspace_1.6.1\F769-FlashFS\synlib\Inc" -I"C:\Users\mbutsch\STM32CubeIDE\workspace_1.6.1\syntalk\c" -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb
2021-06-28 12:53 PM
> the strcat of "1" works, but the strcat of "2" hard faults.
How do you know?
> FreeRTOS
What about stack overflow?
JW
2021-06-28 1:16 PM
I've posted a couple of Hard Fault Handlers that output actionable data. Interested in a full register complement, and fault location.
I'm not sure the STRH will fail inherently due to an odd address, make sure the strlen() hasn't failed due to missing NUL
2021-06-28 1:35 PM
when I singlestep (instruction mode) through the code, inspecting the variable s1....
strcpy(s1, "--"); yields s1 == "--"
strcat(s1, "1"); yields s1 == "--1"
strcat(s1, "2"); yields hard fault when it executes 'strh r3, [r2, #0]'
here are registers after hard fault
pulFaultStackAddress uint32_t * 0x20002390 <ucHeap+5360>
r0 volatile uint32_t 0x3 (Hex)
r1 volatile uint32_t 0x801d45c (Hex)
r2 volatile uint32_t 0x200023cf (Hex)
r3 volatile uint32_t 0x32 (Hex)
r12 volatile uint32_t 0xa (Hex)
lr volatile uint32_t 0x800adb3 (Hex)
pc volatile uint32_t 0x800adc4 (Hex)
psr volatile uint32_t 0x21000000 (Hex)
2021-06-28 1:46 PM
where have you posted Hard Fault Handlers? They may be better than what I have in place currently.
2021-06-28 2:37 PM
https://community.st.com/s/question/0D50X0000BACfzTSQT/how-do-i-debug-a-hard-fault-on-a-stmf7
2021-06-28 2:44 PM
Giving the depressingly awful search afforded by SalesForce (a multi-billion dollar outfit..)
https://github.com/cturvey/RandomNinjaChef/blob/main/KeilHardFault.c
2021-06-28 3:20 PM
> pc volatile uint32_t 0x800adc4 (Hex)
That's not in the region you provided the disasm for above.
0x200023cf is in DTCM. Cortex-M7 should allow unaligned accesses there, unless you've set that area as Device or Strongly Ordered in MPU, or you've disabled unaligned accesses generally by setting SCB_CCR.UNALIGN_TRP.
JW