‎2019-05-27 11:43 PM
Hi I need some help,
I am having the same problem using CubeIDE v1.0. I have copied the arm_math.h, const_structs.h and arm_common_tables.h into Drivers/CMSIS/DSP/Include.
I was not able to find arm_math.h until I went to Project > Properties > C/C++ General > Paths and Symbols > Includes and added in Drivers/CMSIS/DSP/Include. That fixed the problem of not finding arm_math.h
After which I get a whole bunch of errors:
__uint32_t
../Drivers/CMSIS/DSP/Include/arm_math.h:6612:3: error: unknown type name 'uint32_t'; did you mean '__uint32_t'?
uint32_t blockSize);
...
...
../Drivers/CMSIS/DSP/Include/arm_math.h:6873:16: error: unknown type name '__STATIC_INLINE'
CMSIS_INLINE __STATIC_INLINE q15_t arm_bilinear_interp_q15(
^~~~~~~~~~~~~~~
../Drivers/CMSIS/DSP/Include/arm_math.h:6873:38: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'arm_bilinear_interp_q15'
CMSIS_INLINE __STATIC_INLINE q15_t arm_bilinear_interp_q15(
^~~~~~~~~~~~~~~~~~~~~~~
../Drivers/CMSIS/DSP/Include/arm_math.h:6951:16: error: unknown type name '__STATIC_INLINE'
CMSIS_INLINE __STATIC_INLINE q7_t arm_bilinear_interp_q7(
^~~~~~~~~~~~~~~
Thanks!
‎2019-07-21 07:15 PM
I got rid of the (check __FPU_PRESENT) error in my comments above. Did you try it?
"This seems to go away if I include main.h which includes "stm32f4xx_hal.h" before I include "arm_math.h""
‎2019-07-21 07:21 PM
in main.c right?
#include "main.h"
#include "arm_math.h"
And I get:
In file included from C:/Users/alire/OneDrive/Desktop/New folder/1/Drivers/CMSIS/DSP/Include/arm_math.h:319:0,
from ../Drivers/CMSIS/DSP/Source/TransformFunctions/arm_cfft_q15.c:29:
../Drivers/CMSIS/Include/core_cm7.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
#error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
^~~~~
In file included from C:/Users/alire/OneDrive/Desktop/New folder/1/Drivers/CMSIS/DSP/Include/arm_math.h:319:0,
from ../Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.c:29:
../Drivers/CMSIS/Include/core_cm7.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
#error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
^~~~~
In file included from C:/Users/alire/OneDrive/Desktop/New folder/1/Drivers/CMSIS/DSP/Include/arm_math.h:319:0,
from ../Drivers/CMSIS/DSP/Source/TransformFunctions/arm_cfft_f32.c:29:
../Drivers/CMSIS/Include/core_cm7.h:105:8: error: #error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
#error "Compiler generates FPU instructions for a device without an FPU (check __FPU_PRESENT)"
^~~~~
make: *** [Drivers/CMSIS/DSP/Source/TransformFunctions/subdir.mk:118: Drivers/CMSIS/DSP/Source/TransformFunctions/arm_cfft_q15.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Drivers/CMSIS/DSP/Source/TransformFunctions/subdir.mk:112: Drivers/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.o] Error 1
make: *** [Drivers/CMSIS/DSP/Source/TransformFunctions/subdir.mk:116: Drivers/CMSIS/DSP/Source/TransformFunctions/arm_cfft_f32.o] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
‎2019-07-21 07:50 PM
Hmm... I am not sure then. I only did those 2 things. I did not include the DSP/Source folder for my project. Only the Include.
I just tried adding DSP/Source to my project and I got a whole bunch of errors. I managed to get rid of it, by putting
#include "main.h" inside arm_math.h
#ifndef _ARM_MATH_H
#define _ARM_MATH_H
#include "main.h"
I managed to compile fine after that.
‎2019-07-21 08:05 PM
I was thinking that you have done it in main.c
I just did what you explained above and now mine is working too.
I noticed the issue is that arm_math.h gets included before everything else. I changed the order of the directories but still did not solve the issue.
But anyway man, thank you so much for your help. :) Without you this would be impossible.
‎2019-07-21 08:19 PM
Yea I did it in main.c. I didn't include DSP/Source in my project. I only include DSP/Include. Supposedly we don't need to include source, unless we are rebuilding the libraries.
DSP arm_math.h need __FPU_PRESENT to be defined, hence this can be resolved by including "main.h" before including "arm_math.h"
As __FPU_PRESENT is defined in "stm32f407xx.h" > "stm32f407xx.h" > "stm32f4xx_hal_def.h >"stm32f4xx_hal_cortex.h" > "stm32f4xx_hal_conf.h > "stm32f4xx_hal.h"
Its just I noticed you included DSP/Source, which I only managed to resolve the errors from that if I include "main.h" inside "arm_math.h" otherwise, you will need to include "main,h" in every source file that includes "arm_math.h"
Glad to help. =)
‎2019-07-21 08:23 PM
I did not include the sources also. But still i got the error.
including the main.h in ARM_MATH.h solved the issue for me but I will try to see if there is a better workaround without touching the library files. Although this is already great! I have spend more than 24 hours on this.
Thanks again!
‎2019-07-21 09:56 PM
Your log looks like the DSP/Source is included in your project somehow, as the errors came up when you tried to build them.
Maybe it was added as a source folder accidentally?
Glad I could help. :)
‎2019-07-21 09:56 PM
Your log looks like the DSP/Source is included in your project somehow, as the errors came up when you tried to build them.
Maybe it was added as a source folder accidentally?
Glad I could help. =)
‎2019-07-22 02:14 AM
Man you were absolutely right. I was very sleepy (24 hours without sleep) at the time of writing. I had the DSP files located under the project's CMSIS folder and as you may know the project directory is searched for sources by default. (Okay, to be honest I feel stupid :D ). Anyway thank you for all your time and effort. I am going to write a step by step guide for future readers to save them some time and also cover the issue I was facing so they do not fall for this trap like I did.
Thank you again, you saved the day for me and for many other people.:smiling_face_with_heart_eyes: :folded_hands:
‎2019-07-22 03:12 PM
I think I celebrated too early! :D
When I remove the accidentally added files in the source, I get undefined error reference for functions in arm_math.h
C:/Users/alire/OneDrive/Desktop/Testing Fir FIlter/Stage1/Debug/../Src/main.c:234: undefined reference to `arm_fir_init_f32'
C:/Users/alire/OneDrive/Desktop/Testing Fir FIlter/Stage1/Debug/../Src/main.c:238: undefined reference to `arm_fir_f32'
I think I am doing something stupid again :D but cannot figure it out. On the bright side when I include the source things get compiled and run correctly.