2023-08-15 2:05 AM
Updating the cubeide generates this error:
An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Result of processing steps.
OK
OK
OK
Public key not found for 70b824d9a6b4ae29.
OK
I could just intall the latest version, but I assume there is a way to fix this.
Thanks,
Jamie
Solved! Go to Solution.
2023-08-18 5:25 AM
Hello @j1s1e1 ,
Thank you for your contributions and for your detailed explanations.
The issue has been reported to STM32CubeIDE development team.
Internal ticket number: 159507(This is an internal tracking number and is not accessible or usable by customers).
I will keep you posted with updates, and I hope that this answered your question.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Regards,
Rim
2023-08-15 2:49 AM - edited 2023-08-15 3:33 AM
2023-08-15 6:22 PM
Hi Rim --
I have STM Cube IDE 1.9.0. I see upgrades that go up to 1.13.0. I did try both update to latest and update to next in case multiple steps were required. Additional details are listed below.
Thanks,
Jamie
*** Platform Details:
*** System properties:
applicationXMI=org.eclipse.ui.workbench/LegacyIDE.e4xmi
awt.toolkit=sun.awt.windows.WToolkit
ds.delayed.keepInstances=true
ds.delayed.keepInstances.default=true
eclipse.application=org.eclipse.ui.ide.workbench
eclipse.buildId=Version 1.9.0
eclipse.commands=-os
win32
-ws
win32
-arch
x86_64
-showsplash
-launcher
2023-08-17 5:57 AM
I have the same problem. Do you have solution?
2023-08-18 5:25 AM
Hello @j1s1e1 ,
Thank you for your contributions and for your detailed explanations.
The issue has been reported to STM32CubeIDE development team.
Internal ticket number: 159507(This is an internal tracking number and is not accessible or usable by customers).
I will keep you posted with updates, and I hope that this answered your question.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Regards,
Rim
2023-09-08 8:16 AM
Why is this marked as "solved"? The accepted solution has no useful information other than "we know about the problem and will keep you updated." How about an update? The least you could've done is provide the link to download the latest CubeIDE installer, which is here (requires STM login or PII).
#metoo also with CubeIDE 1.9.0
An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Result of processing steps.
OK
OK
OK
Public key not found for 70b824d9a6b4ae29.
OK
2023-09-29 7:23 PM
I also have CubeIDE update problem. However, the error is different.
An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Problems downloading artifact: osgi.bundle,org.eclipse.equinox.common,3.17.100.v20230202-1341.
Error reading signed content:C:\Users\xxx\AppData\Local\Temp\signatureFile9190832969811238731.jar
An error occurred while processing the signatures for the file: C:\Users\xxx\AppData\Local\Temp\signatureFile9190832969811238731.jar
Problems downloading artifact: osgi.bundle,org.eclipse.text.quicksearch,1.1.500.v20230129-1959.
Error reading signed content:C:\Users\xxx\AppData\Local\Temp\signatureFile5145962442517373072.jar
An error occurred while processing the signatures for the file: C:\Users\xxx\AppData\Local\Temp\signatureFile5145962442517373072.jar
My CubeIDE is build info:
STM32CubeIDE
Version: 1.7.0
Build: 10852_20210715_0634 (UTC)
OS: Windows 10, v.10.0, x86_64 / win32
Java version: 11.0.10
2024-01-21 4:51 PM
Same problem with Update to IDE 14.
An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Result of processing steps.
OK
OK
Public key not found for 5c28247a08c3bba7.
OK
Result of processing steps.
OK
OK
Public key not found for 5c28247a08c3bba7.
OK
2024-10-29 4:01 PM
This is not a solution and the problem still exists.
Is there a solution?
In what world does "The issue has been reported to STM32CubeIDE development team" equal "this answered your question"
2024-10-30 7:20 AM
tl;dr: The solution is to manually download and install the latest Cube package.
I suspect this is a situation where the old version has a baked-in key or GUID or something that isn't valid anymore. Since that breaks its ability to fetch updates in the first place, that means it necessarily requires user intervention to correct.
Why ST decided to unpublish the public key for 5c232.... in the first place is another question entirely; perhaps some security issue? Or perhaps that identifier was just wrong from the start and ST can't publish something that fixes it without breaking something else (such as violating uniqueness, if the identifier was wrong).
In any case, yes, the "accepted answer" is not an answer. Thanks for the kudos!