cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to upload code via st link v2 on stm32h725vgt6

AmitUpadhyay
Associate II

Sir

We are not able to program the stm32h725vgt6 board.We got some issues and in order to rectify the issue  we have connected  VDDSMPS and VFBSMPS to the GND and voltage on the VCAP ia about 1V for supply 3.3V V. But still unable to program the board.

Failed to execute MI command:
target remote localhost:61234

Error message from debugger back end:
localhost:61234: Connection timed out.
Failed to execute MI command:
target remote localhost:61234

Error message from debugger back end:
localhost:61234: Connection timed out.
localhost:61234: Connection timed out.

2 REPLIES 2
Andrew Neil
Super User

How to solve connection errors when connecting and programming the STM32 target board.

How to solve debugger connection issues


@AmitUpadhyay wrote:

the stm32h725vgt6 board..


What board ?

How to write your question to maximize your chances to find a solution

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User

Is this a custom board? Has the board ever worked?

If you've set the wrong power mode, see here:

How to unbrick an STM32H7 after setting the wrong ... - STMicroelectronics Community

 

If you feel a post has answered your question, please click "Accept as Solution".