cancel
Showing results for 
Search instead for 
Did you mean: 

unable to receive data on USART3 using DMA

debug
Associate III

Hi,

I need to configure DMA for the Rx path of my USART data. I was able to get the Tx path going correctly following this thread: https://community.st.com/t5/stm32cubeide-mcus/problem-adding-usart3-functionality-to-lwip-http-server-netconn/m-p/668703#M26841

Now for the Rx path, the DMA gets setup in HAL_UART_MspInit() & this was copied as generated by CubeMX, i.e. and it's working on the other project (with CubeMX enabled) fine:

else if(huart->Instance==USART3)
{
/* Peripheral clock enable */
__HAL_RCC_USART3_CLK_ENABLE();

__HAL_RCC_GPIOD_CLK_ENABLE();
/**USART3 GPIO Configuration
PD8 ------> USART3_TX
PD9 ------> USART3_RX
*/
GPIO_InitStruct.Pin = XZaber_TX_Pin|XZaber_RX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

/* USART3 DMA Init */
/* USART3_RX Init */
hdma_usart3_rx.Instance = DMA1_Stream1;
hdma_usart3_rx.Init.Channel = DMA_CHANNEL_4;
hdma_usart3_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_usart3_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_usart3_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_usart3_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_usart3_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_usart3_rx.Init.Mode = DMA_CIRCULAR;
hdma_usart3_rx.Init.Priority = DMA_PRIORITY_LOW;
hdma_usart3_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_usart3_rx) != HAL_OK)
{
Error_Handler();
}

__HAL_LINKDMA(huart,hdmarx,hdma_usart3_rx);

/* USART3 interrupt Init */
HAL_NVIC_SetPriority(USART3_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(USART3_IRQn);
}

  Now in my project without CubeMX, I'm explicitly starting the DMA clocks by calling : __HAL_RCC_DMA1_CLK_ENABLE() and also the following lines are called too during init:

 rv = HAL_UART_Receive_DMA(&huart1, OMRxDat, OM20_MEAS_GET_RXLEN);
rv = HAL_UART_Receive_DMA(&huart3, ZabRxDat, sizeof(ZabRxDat));

I can see that data is coming in on the scope (as a reply to what I send out) but none of the callbacks get invoked. I am checking UART_DMAReceiveCplt(), UART_DMARxHalfCplt & UART_DMAError(). What am I missing for the callback in my program void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) to kick in when data is received?

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Try to inspire from one of examples using DMA like this one: https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM324x9I_EVAL/Examples/UART/UART_Hyperterminal_DMA

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

2 REPLIES 2
SofLit
ST Employee

Try to inspire from one of examples using DMA like this one: https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM324x9I_EVAL/Examples/UART/UART_Hyperterminal_DMA

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Excellent, Thanks with the information found in this link I was able to get it going!