cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to read NAND flash ID

ashutoshtekriwal
Associate II

Hello,

We have been using NAND Flash (MT29F8G08ADAFAH4-AAT) interfaced with STM32L562 microcontroller using FMC interface. We are first trying to read the ID of the Flash using the below HAL API.

 

if(HAL_NAND_Read_ID(&hnand1, &NAND_ID) != HAL_OK)

{

return NAND_STATUS_READ_ID_ERROR;

}

 

But it is returning a read ID error. The section for the NAND initialization using FMC interfcace is provided below:

Please provide us some help.

 

 

/* FMC initialization function */

static void MX_FMC_Init(void)

{

 

/* USER CODE BEGIN FMC_Init 0 */

 

/* USER CODE END FMC_Init 0 */

 

FMC_NAND_PCC_TimingTypeDef ComSpaceTiming = {0};

FMC_NAND_PCC_TimingTypeDef AttSpaceTiming = {0};

 

/* USER CODE BEGIN FMC_Init 1 */

 

/* USER CODE END FMC_Init 1 */

 

/** Perform the NAND1 memory initialization sequence

*/

hnand1.Instance = FMC_NAND_DEVICE;

/* hnand1.Init */

hnand1.Init.NandBank = FMC_NAND_BANK3;

hnand1.Init.Waitfeature = FMC_NAND_WAIT_FEATURE_DISABLE;

hnand1.Init.MemoryDataWidth = FMC_NAND_MEM_BUS_WIDTH_8;

hnand1.Init.EccComputation = FMC_NAND_ECC_DISABLE;

hnand1.Init.ECCPageSize = FMC_NAND_ECC_PAGE_SIZE_256BYTE;

hnand1.Init.TCLRSetupTime = 0;

hnand1.Init.TARSetupTime = 0;

/* hnand1.Config */

hnand1.Config.PageSize = 4096;

hnand1.Config.SpareAreaSize = 256;

hnand1.Config.BlockSize = 64;

hnand1.Config.BlockNbr = 2048;

hnand1.Config.PlaneNbr = 2;

hnand1.Config.PlaneSize = 2048;

hnand1.Config.ExtraCommandEnable = DISABLE;

/* ComSpaceTiming */

ComSpaceTiming.SetupTime = 223;

ComSpaceTiming.WaitSetupTime = 223;

ComSpaceTiming.HoldSetupTime = 224;

ComSpaceTiming.HiZSetupTime = 223;

/* AttSpaceTiming */

AttSpaceTiming.SetupTime = 223;

AttSpaceTiming.WaitSetupTime = 223;

AttSpaceTiming.HoldSetupTime = 224;

AttSpaceTiming.HiZSetupTime = 223;

 

if (HAL_NAND_Init(&hnand1, &ComSpaceTiming, &AttSpaceTiming) != HAL_OK)

{

Error_Handler( );

}

 

/* USER CODE BEGIN FMC_Init 2 */

 

/* USER CODE END FMC_Init 2 */

}

 

1 REPLY 1
KDJEM.1
ST Employee

Hello @ashutoshtekriwal ,

 

 Could you please make sure that the FMC is correctly configured for the NAND "MT29F8G08ADAFAH4-AAT"  Flash. 

May this application note can help you to check memory protection unit (MPU).

Also may you facing a hardware issue, for that please verify that all the necessary pins for the NAND interface are correctly configured and connected.

 

I hope this help you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.