User Activity

I am using STM32L562 family microcontroller. I have interfaced TCPP01-M12 with my microncontroller. I have a doubt , whether i can use this device when using UCPD in source mode, as i am unable to configure software packages for source mode(X-CUBE-TC...
Hello,We have been using NAND Flash (MT29F8G08ADAFAH4-AAT) interfaced with STM32L562 microcontroller using FMC interface. We are first trying to read the ID of the Flash using the below HAL API. if(HAL_NAND_Read_ID(&hnand1, &NAND_ID) != HAL_OK){retur...
Hello,We have interfaced a NOR flash (S26KL512SDABHN020) with STM32L562 over OctoSPI in Hyperbus mode. The Low level drivers were found from one of the forums of ST community and were ported in our code. We are unable to read/write data at the base a...
Hello,We have been using two SRAMs (CY7C1061G30-10BV1XE) & one NAND Flash(MT29F8G08ADAFAH4-AAT) interfaced with STM32L562 micro-controller on same FMC bus. We have initialised FMC and try to access SRAM1 by selecting Chip select: NE1 and Bank 1. It i...
Kudos from