2024-05-02 9:37 AM
When moving to the latest LTS version of Ubuntu (version 24.04), I received the following message when attempting to install Cube IDE and after accepting all of the license agreements:
The following packages have unmet dependencies:
st-stm32cubeide-1.15.1 : Depends: libncurses5 but it is not installable
Depends: libpython2.7 but it is not installable
Depends: libwebkit2gtk-4.0-37 but it is not installable
E: Unable to correct problems, you have held broken packages.
After running "sudo apt-cache search" for each of these packages, I found the following:
for libncurses5 only libncurses-dev was returned. The version associated with 24.04 is (6.4+20240113-1ubuntu2)
for libpython2.7 nothing was returned and when I searched for just libpython only libpython3-all-dev and its associated packages were listed.
for libwebkit2gtk-4.0-37 nothing was returned but when searching for libwebkit2gtk version libwebkit2gtk-4.1 was returned.
Are there plans to update Cube IDE soon to use updated libraries?
Solved! Go to Solution.
2024-05-21 7:14 AM
I meant when I try to flash the board. Apparently, Only Ubuntu 20.04 - 22.04 are supported. Ubuntu 24.04 is not supported.
2024-05-22 5:45 AM
Dear all
I managed to get STM32CubeIDE 1.15.1 running on Ubuntu 24.04. I used the "Generic Linux" installer, not the Debian one. I was able to manually download and install libtinfo5_6.4-4_amd64.deb and libncurses5_6.4-4_amd64.deb
Importing a project, building and running and even the ST login seems to work properly.
But when I try to load an IOC file it fails without any error message, only a gray background is displayed.
However as a workaround I was able to load, edit and generate code using the "standalone version" Cube MX.
I hope that ST will soon fix CubeIDE to properly run on Ubuntu 24.04 "out of the box".
2024-05-22 7:16 AM
Same here, Use generic 1.12.0, it's working properly here.
2024-06-06 2:41 AM
I assume that I am experiencing the same as @trusty, being unable to upload firmware to the MCU. I have created a separate topic for it here: https://community.st.com/t5/stm32cubeide-mcus/unable-to-upload-firmware-on-ubuntu-24-04/td-p/683268
2024-08-06 12:41 AM
GDB works after download and install ncurses5. Try this:
wget http://archive.ubuntu.com/ubuntu/pool/universe/n/ncurses/libtinfo5_6.4-2_amd64.deb && sudo dpkg -i libtinfo5_6.4-2_amd64.deb && rm -f libtinfo5_6.4-2_amd64.deb
wget http://archive.ubuntu.com/ubuntu/pool/universe/n/ncurses/libncurses5_6.4-2_amd64.deb && sudo dpkg -i libncurses5_6.4-2_amd64.deb && rm -f libncurses5_6.4-2_amd64.deb
2024-08-29 12:30 AM
I just boot my new desktop with ubuntu24.04, and seems generic_linux download version is the best to operate.
Also, I keep getting the error during flashing/debugging the chip, it reports
"Could not determine GDB version using command: arm-none-eabi-gdb --version arm-none-eabi-gdb: /lib/x86_64-linux-gnu/libncurses.so.5: version NCURSES_5.3.20021019' not found (required by arm-none-eabi-gdb) arm-none-eabi-gdb: /lib/x86_64-linux-gnu/libncurses.so.5: version NCURSES_5.1.20000708' not found (required by arm-none-eabi-gdb) arm-none-eabi-gdb: /lib/x86_64-linux-gnu/libncurses.so.5: version NCURSES_5.6.20061217' not found (required by arm-none-eabi-gdb) arm-none-eabi-gdb: /lib/x86_64-linux-gnu/libncurses.so.5: version NCURSES_5.0.19991023' not found (required by arm-none-eabi-gdb) arm-none-eabi-gdb: /lib/x86_64-linux-gnu/libtinfo.so.5: version NCURSES_TINFO_5.0.19991023' not found (required by arm-none-eabi-gdb)"
I solved it according to following operations.
1. Manually download the required libtinfo5 package which is the dependency of libncurses5. https://launchpad.net/ubuntu/lunar/amd64/libtinfo5/6.4-2
2. cd into your download directory, setting up the libtinfo5 package "sudo dpkg -i libtinfo5_6.4-2_amd64.deb"
3. then "curl -O http://launchpadlibrarian.net/648013227/libncurses5_6.4-2_amd64.deb" to get the libncurses5
4. set up the libncurses5 package "sudo dpkg --configure libncurses5:amd64"
5. all good~
2024-10-03 7:21 AM
I had the same problem with Cube IDE 1.16.1 installation on Lubuntu 24.04 , the lightweight version of desktop Ubuntu 24.04.
By apply the Generic Linux installation, it seems went success.
Basically the installation went to /opt/st/stm32cubeide_1.16.1/ , and external gnu tools it uses to be installed under /opt/st/stm32cubeide_1.16.1/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.linux64_1.0.200.202406132123/ .
The arm-none-eabi-gcc --version shows as
--------------------------------------------------------------------------------------------------------------------
arm-none-eabi-gcc (GNU Tools for STM32 12.3.rel1.20240612-1315) 12.3.1 20230626
Copyright (C) 2022 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
------------------------------------------------------------------------------------------------------------------------
looks like a ST customized build for STM32.
When look to `arm-none-eabi-gdb --version` , it complains with
--------------------------------------------------------------------------------------------------------------------------
arm-none-eabi-gdb: /lib/x86_64-linux-gnu/libtinfo.so.5: version `NCURSES_TINFO_5.5.20051010' not found (required by /lib/x86_64-linux-gnu/libncurses.so.5)
--------------------------------------------------------------------------------------------------------------------------
This makes me to be somewhat to worry if the debug session in Cube IDE would start properly.
There is a little bit background info that the newer gnu arm tool package does not include arm-none-eabi-gdb, rather then it suggested to use gdb-multiarch. So if you had encountered a problem to start gdb session through arm-none-eabi-gdb , try to install linux/ubuntu package of gdb-multiarch, and then tweak the settings in Cube IDE to use gdb-multiarch rather than arm-none-eabi-gdb to start gdb session.
If for whatever reason want to keep using arm-none-eabi-gdb , then have to solve libncurses.so.5 issue. On newer Linux/Ubuntu release, only libncurses.so.6 provided, so either to create link for ncurses.so.5 point to ncurses.so.6, or pull a real version of ncurses.so.5 from an older version of Linux/Ubuntu release, and put them into /lib/x86_64-linux-gnu/. So the hack to be something like
-------
rsync old_ubuntu_host:/lib/x86_64-linux-gnu/libtinfo.so.5.9 ./
sudo rsync libtinfo.so.5.9 /lib/x86_64-linux-gnu/
rsync old_ubuntu_host:/lib/x86_64-linux-gnu/libncurses.so.5.9 ./
sudo rsync libncurses.so.5.9 /lib/x86_64-linux-gnu/
sudo ln -s /lib/x86_64-linux-gnu/libtinfo.so.5.9 /lib/x86_64-linux-gnu/libtinfo.so.5
sudo ln -s /lib/x86_64-linux-gnu/libncurses.so.5.9 /lib/x86_64-linux-gnu/libncurses.so.5
-------
or
-----
sudo ln -s /lib/x86_64-linux-gnu/libtinfo.so.6.4 /lib/x86_64-linux-gnu/libtinfo.so.5
sudo ln -s /lib/x86_64-linux-gnu/libncurses.so.6.4 /lib/x86_64-linux-gnu/libncurses.so.5
------
The arm-none-eabi-xxx under /usr/bin/ may use globally, so feel free to create link there to point to a specific version of arm-none-eabi installation,if you have multiple versions installed.
My fellow developers, happy hacking! Share your experience!
2024-11-28 1:43 AM
What i did on my Ubuntu 24 Install :-
Types: deb
URIs: http://security.ubuntu.com/ubuntu
Suites: focal-security
Components: main universe
Signed-By: /usr/share/keyrings/ubuntu-archive-keyring.gpg
2025-01-07 2:57 AM
Finally, that did the trick.
I searched for this several days.
God bless you!
Instead of point 4. (set up) I had to install: "sudo dpkg -i libncurses5_6.4-2_amd64.deb"
2025-01-12 2:04 AM
HI,
3 First steps from cwang.13
4th from MichaelRuck
And it is OK
just a link (ln) from ncurse6 doesn't work !!!
BR
JP