2024-05-02 9:37 AM
When moving to the latest LTS version of Ubuntu (version 24.04), I received the following message when attempting to install Cube IDE and after accepting all of the license agreements:
The following packages have unmet dependencies:
st-stm32cubeide-1.15.1 : Depends: libncurses5 but it is not installable
Depends: libpython2.7 but it is not installable
Depends: libwebkit2gtk-4.0-37 but it is not installable
E: Unable to correct problems, you have held broken packages.
After running "sudo apt-cache search" for each of these packages, I found the following:
for libncurses5 only libncurses-dev was returned. The version associated with 24.04 is (6.4+20240113-1ubuntu2)
for libpython2.7 nothing was returned and when I searched for just libpython only libpython3-all-dev and its associated packages were listed.
for libwebkit2gtk-4.0-37 nothing was returned but when searching for libwebkit2gtk version libwebkit2gtk-4.1 was returned.
Are there plans to update Cube IDE soon to use updated libraries?
Solved! Go to Solution.
2024-05-03 9:17 AM
I had the same issue on my Ubuntu 24.
I saw at https://www.st.com/en/development-tools/stm32cubeide.html#get-software another linux version (STM32CubeIDE Generic Linux Installer) and I was able to install it.
For now it seems to be working fine.
2024-05-03 1:43 AM
I have the Same Problem :expressionless_face:
2024-05-03 8:25 AM
Who still uses python 2.7 in 2024?! Python 2.7 has been discontinued since January 2020... I have used STM32CubeIDE on Ubuntu in the past without any serious issues (aside from scaling issues, but I've had scaling issues on Windows too), but not on 24 yet.
2024-05-03 9:17 AM
I had the same issue on my Ubuntu 24.
I saw at https://www.st.com/en/development-tools/stm32cubeide.html#get-software another linux version (STM32CubeIDE Generic Linux Installer) and I was able to install it.
For now it seems to be working fine.
2024-05-11 1:07 PM
Does it worked? I can't login :(
2024-05-15 6:20 AM - edited 2024-05-15 6:21 AM
I was able to install the CubeIDE from the Generic Linux option, but cannot login to myST. I'm on Ubuntu 24.04, tried versions 1.15.1 and 1.14.0, but cannot login too.
2024-05-20 6:42 AM
Apparently, logging in from the CubeIDE works right now.
But I also experience the problem that I cannot run an example project because it is looking for libncurses5 whereas this Ubuntu only has the libncurses6.
2024-05-20 6:59 AM
I tested all versions, login and compile/debug just working on 1.12.0
2024-05-20 4:32 PM
Even if you were able to install there are still problems down the line due to libncurses5. I was able to install on Ubuntu 24.04 using the generic Linux Installer, but I cannot load jobs to my MCU.
Could not determine GDB version using command: arm-none-eabi-gdb --version
arm-none-eabi-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or directory
I cannot get proceed beyond this at the moment.
2024-05-21 12:15 AM
What do you mean by "load jobs to my MCU"?