2023-04-27 07:50 AM
I am trying to display UART data received to UI WITHOUT RTOS but I am unsure how to code the model, I am getting error every time. I read the documentation and tried to reproduce the same thing but in vain. I watched a lot of videos on youtube but they all used RTOS. My project consists of not using RTOS.
I can confirm that my UART works and I can receive strings from a terminal. I used HAL UART function in the Main() while loop.
while (1)
{
MX_TouchGFX_Process();
HAL_UARTEx_ReceiveToIdle_DMA(&huart3, RX_String, sizeof(RX_String));
}
In my Screen1View.cpp file, I have inserted a function that should display the received UART string to a text box:
void Screen1View::uart_Data(char* RX_String)
{
textArea2.setWideTextAction(touchgfx::WIDE_TEXT_WORDWRAP);
Unicode::strncpy(textArea2Buffer, RX_String, TEXTAREA2_SIZE);
textArea2.invalidate();
}
In the Screen1Present.cpp:
void Screen1Presenter::uart_Data(char* RX_String)
{
view.uart_Data(RX_String);
}
I declared virtual void uart_Data(char* RX_String); in ModelListener.hpp
I am however having problem with Model.cpp:
void Model::tick()
{
#ifndef SIMULATOR
modelListener->uart_Data(RX_String);
#endif
}
This is what I have so far and I feel something is missing. Can someone please give some guidance?
Solved! Go to Solution.
2023-04-28 10:59 AM
OK, as far as I see you should replace
virtual void uart_Data(char* RX_String);
with
virtual void uart_Data(char* RX_String){}
in ModelListener.hpp.
Attached is tested simple example files from model tick to view. Remember to set typography wildcard range for exmpale 0x00-0xff. You can also touchgfx_printf- functions in simulator to test execution (commented)
2023-04-27 07:51 AM
My Error is:
c:\st\stm32cubeide_1.11.2\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe: ./Application/User/gui/Screen1Presenter.o: in function `ModelListener::ModelListener()':
C:/Users/o.sang/Documents/TouchGFX/LED_toggle_UART1/STM32CubeIDE/CM7/Debug/../../CM7/../../CM7/TouchGFX/gui/include/gui/model/ModelListener.hpp:9: undefined reference to `vtable for ModelListener'
c:\st\stm32cubeide_1.11.2\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\bin\ld.exe: ./Application/User/gui/Screen1Presenter.o: in function `ModelListener::~ModelListener()':
C:/Users/o.sang/Documents/TouchGFX/LED_toggle_UART1/STM32CubeIDE/CM7/Debug/../../CM7/../../CM7/TouchGFX/gui/include/gui/model/ModelListener.hpp:11: undefined reference to `vtable for ModelListener'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:90: stm32h745i_disco_CM7.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
2023-04-27 09:39 AM
Where you have define the RX_String which main.cpp uses and have you extern it to the model.cpp or how the model.cpp knows it ?
2023-04-28 12:36 AM
Do you mean main.c? Because I do not see any main.cpp file in my project folder. In main.c, RX_String is defined as:
uint8_t RX_String[257];
which is being used in the while loop by a HAL UART function.
For the extern to model.cpp, I wrote the following but I am not sure if that's correct:
#ifndef SIMULATOR
#include "main.h"
#endif
extern "C"
{
extern char* RX_String[];
}
2023-04-28 07:24 AM
primary you can , but this isnt good on every tick update (check change)
secondary your extern is bad
use
extern uint8_t RX_String[];
and screenpresenter.hpp need too add
virtual void uart_data...
and in both send pointer to string declared global is waste of params.
2023-04-28 10:59 AM
OK, as far as I see you should replace
virtual void uart_Data(char* RX_String);
with
virtual void uart_Data(char* RX_String){}
in ModelListener.hpp.
Attached is tested simple example files from model tick to view. Remember to set typography wildcard range for exmpale 0x00-0xff. You can also touchgfx_printf- functions in simulator to test execution (commented)
2023-05-02 06:21 AM
Thank you for your answer!
After removing the semicolon ; and replacing it with {}, the error was gone and I was able to compile and it now displays string from UART!
I don't get however why replacing the semicolon with {} made it work...if someone or you could explain me, would be great!
2023-05-02 10:44 AM
Good that you get forward👍
This line is not function prototype, but it defines (this case empty) virtual function to the modelListener- class. This virtual function is then overrided in presenter class, you can see the prototype in presenter.hpp and function presenter.cpp.
Maybe you have allready read this documentation:
2024-02-02 05:28 AM
Hi,
indeed, it helps to put {} after my own virtual function definition
Achim