Timer 8 issue in Cube IDE V1.5.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-27 10:47 PM
When generating Code for STM32H753IIKx I recently stumbled across unexpected behaviour in Cube IDE V1.5.0. I'm using the processor Pins PH13-PH15 in order to output a PWM Signal from the N-Outputs of Timer 8 (CH1N1-3). However no correlating signals were observed.
My timer initialization:
static void MX_TIM8_Init(void)
{
/* USER CODE BEGIN TIM8_Init 0 */
/* USER CODE END TIM8_Init 0 */
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM8_Init 1 */
/* USER CODE END TIM8_Init 1 */
htim8.Instance = TIM8;
htim8.Init.Prescaler = 2000-1;
htim8.Init.CounterMode = TIM_COUNTERMODE_UP;
htim8.Init.Period = 255-1;
htim8.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim8.Init.RepetitionCounter = 0;
htim8.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_PWM_Init(&htim8) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim8, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 255-1;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
sBreakDeadTimeConfig.Break2Filter = 0;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim8, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM8_Init 2 */
HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_1);
HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_2);
HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_3);
HAL_TIM_PWM_Start_DMA(&htim8, TIM_CHANNEL_1, (uint32_t*)&RGB_array[0], 1);
HAL_TIM_PWM_Start_DMA(&htim8, TIM_CHANNEL_2, (uint32_t*)&RGB_array[1], 1);
HAL_TIM_PWM_Start_DMA(&htim8, TIM_CHANNEL_3, (uint32_t*)&RGB_array[2], 1);
/* USER CODE END TIM8_Init 2 */
HAL_TIM_MspPostInit(&htim8);
}
Cube IDE Setting:
Further investigation showed, that registers for controlling the driver stage were not set accordingly in the peripheral. Only the complementary outputs of the PWM stage were enabled (CH1-3).
Writing to the registers manually later on (outside of the auto-generated codeblock) solved the issue:
htim8.Instance->CCER = (1UL << 2) | (1UL << 6) | (1UL << 10);
Is this a bug or are there underlying mechanics which I'm not realizing?
- Labels:
-
Bug-report
-
STM32CubeIDE
-
STM32H7 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-04 9:55 PM
Does no one have a clue?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-05 12:05 AM
If I well catch, you want only negative or positive + negatiev to control 6 mosfets with dead time? If second, you ahve to enable them in CubeMX.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-05 12:22 AM
The timer is not used for any kind of bridge,... where dead time would be required. We just have a PCB where a RGB LED is routed to the PWM Pins. R, G and B to one Timer channel Pin. Not a huge deal, but I was just wondering what might be wrong here.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-05 3:40 AM
/**
* @brief Enables or disables the TIM Capture Compare Channel xN.
* @param TIMx to select the TIM peripheral
* @param Channel: specifies the TIM Channel
* This parameter can be one of the following values:
* @arg TIM_Channel_1: TIM Channel 1
* @arg TIM_Channel_2: TIM Channel 2
* @arg TIM_Channel_3: TIM Channel 3
* @param ChannelNState: specifies the TIM Channel CCxNE bit new state.
* This parameter can be: TIM_CCxN_ENABLE or TIM_CCxN_Disable.
* @retval None
*/
static void TIM_CCxNChannelCmd(TIM_TypeDef* TIMx, uint32_t Channel, uint32_t ChannelNState)
{
That's quoting from STM32Cube_FW_H7_V1.3.0\Drivers\STM32H7xx_HAL_Driver\Src\stm32h7xx_hal_tim_ex.c . I don't Cube at all, so don't know if this can be somehow clicked in CubeMX.
JW