2024-04-08 3:03 PM
New workspace
New STM32 project
Board Selector Nucleo-144 STM32H5 NUCLEO-H563ZI
Take the defaults
Set the tick to TIM6
Pinout & Configuration - Middleware and Software Packs - THREADX
Generate App Init Code - check
Save everything, compile, debug, put a breakpoint on the opening curly in tx_app_thread_entry (app_threadx.c).
Run and reach the breakpoint.
Window - Show View - ThreadX - ThreadX Thread List
Notice how the names are just the first character of the name strings.
This happens on queues as well. I suspect semaphores and mutexs will be the same.
This worked properly in a previous version of CubeIDE on STM32L4 if that matters.
Full cube project attached.
Solved! Go to Solution.
2024-11-12 4:21 PM
Another interesting data point. I am now using CubeIDE 1.16.1, but with MacOS 15.1 and the labels are now correct.
Perhaps the latest version of MacOS fixed a regression??? Also, I noticed that the Eclipse logo is upside down again, so this could be chasing a MacOS issue.
2024-04-09 3:58 AM
Hello @Andrei Chichak,
Thank you for your valuable inputs
I created an internal ticket to track the issue ( Internal ticket number: 178581)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-11 1:30 PM - edited 2024-04-11 1:46 PM
Yes, I checked a previous project, using a L452 processor, that had the proper names previously and it is now broken.
Also, the names of semaphores, byte pools, message queues, mutexes, event flags, and threads are all truncated.
So, it looks like it is an issue with 1.15.0.
Andrei
2024-05-30 11:27 AM
Just as a data point, I'm also encountering this on 1.15.1, on my H743 project. I'm happy to hear that it's not just me!
2024-05-31 2:29 AM - edited 2024-05-31 2:30 AM
Hello @ron239955_stm1,
Could you give us more details on your environment?
Have you updated the 1.15.1 or installed it from the installation package?
Also, could you provide your log file (console) when this issue happens
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-31 11:38 AM
@Sarra.S the DM system is really badly designed and ... well here is a compressed file with the console log that you were asking for.
2024-06-04 7:20 AM - edited 2024-06-04 7:21 AM
Hello @Andrei Chichak ,
Could you please attach the debug log file so that we can further investigate the issue.
You can find it under the Debug folder after enabling 'log to file' in the Debug configuration as illustrated in the screenshot below:
Thank you,
Souhaib
2024-06-04 9:30 AM
2024-06-04 12:30 PM
@ron239955_stm1 Are you using a Mac, or are you on Windows or Linux?
2024-06-04 1:41 PM
I'm on Mac as well (M3 MacBook Pro, MacOS 14.5)