cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5 - Enable MDF use ADC1 as data source

James613
Associate II

Hello,

Can anyone give me some hints how can I use ADC1 as data source for the MDF?

Thank you

James613_0-1717884308645.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @James613 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to put the Cursor on the greyed Command that set the ADC1 as data source for the MDF (as shown on your screenshot). A message will pop-up to indicate how to make this option available or why you can't configure it. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @James613 and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to put the Cursor on the greyed Command that set the ADC1 as data source for the MDF (as shown on your screenshot). A message will pop-up to indicate how to make this option available or why you can't configure it. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you so much!!!

I don't know this function before. I finally found that I need to change the conversion data management mode of ADC1 to MDF mode and the problem solved