cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H563 & FreeRTOS

DiBosco
Senior

We've designed a board with an H563 on it. Before I started the PCB layout I checked that FreeRTOS was supported for this device and saw it was.

However, now I come to create a project in the Cube IDE it doesn't seem quite so straightforward.

It [the H563 family] wasn't supported in version 1.9 of the IDE so I upgraded to 1.16.

I'm concerned though that FreeRTOS no longer seems to be automatically in Cube's set up ands you seem to have to install this X-CUBE-FREERTOS  add on which seems to suggest though that TCP/IP is not supported. Is that correct?

Also once you've downloaded this add on, how do you actually install it into Cube?

If we need to run FreeRTOS with TCP/IP support is the H563 the wrong processor to be using?

Thanks!

 

 

2 REPLIES 2
AScha.3
Chief II

Now on H563 you have Azure RTOS , with can have FAT , sd-card, USB and network...

AScha3_0-1720635772285.png

But if want freertos, ...tcp/ip - dont know, maybe look here:

https://github.com/FreeRTOS/FreeRTOS-Plus-TCP

https://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_TCP/index.html

 

 

If you feel a post has answered your question, please click "Accept as Solution".
Peter BENSCH
ST Employee

@DiBosco the X-CUBE packages can be installed via the Package Manager:

Help > Manage Embedded Software Packages, tab STMicroelectronics

where you can then select the desired version.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.