cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H533CET6 File download error

Erik_Valente
Associate

Hi everyone,

 

I have problems programming the STM32H533CET6, I get a file download error.

 

 

Error: failed to download Segment[0]
Error: failed to download the File
Encountered Error when opening C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.400.202404281720\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.

 

 

 

I can read the memory and delete it. But I can't download any program. I have already verified that the memory is not protected and the trusted zone is disabled. I also checked the connections according to AN5711.


I tried the “Normal”, “hot plug” and the different reset modes in STM32Programmer.

Nothing works.

Does anyone have an idea what could be the problem?

I use:
ST-link v2
CubeIde: V1.16.1
Programmer: V2.17

Thank you.

2 REPLIES 2
Imen.D
ST Employee

Hello @Erik_Valente ,

This article will help you in case you are using a custom external loader:

Custom external loader "failed to download segment... - STMicroelectronics Community

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Hi, Imen

Thank you for your response. Let me tell you that I am not using an external loader. I chose this H533 to use FD CAN, but I can't even set a port to high ( without delay).
I tried overwriting HAL Tick, as mentioned in the post you mentioned, without success. I get the same result.

Any other idea?

Thanks.