cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411 as usb video input

Tarek Ch.
Associate

I built a project, i'm gathering data from an I2C sensor and display the result on a 2.8" tft screen (connected on SPI)

since STM32F411 has native USB module, i'm want to let the PC recognize the STM32F411 as a webcam (or any video input device)

Any help or guidance to achieve that is appreciated.

Also note that the resolution is going to be maximum 320x240 and a refresh rate of 10-12

1 REPLY 1
Pavel A.
Evangelist III

But basically you want to display only text?