Skip to main content
Visitor II
Jun 19, 2023 6:07 AM UTC
Question

interfacing st4sim-200m with stm32f103 nucleo-64 board

Regarding the  serial communication protocol that I need to use to read and write the data from the module as the st4sim_200m has only one serial I/o port.

in the datasheet it is mentioned that to use SPI . but i not able to find the spi peripheral's like MOSI and MISO pins on the st4sim . 

Can i use stm32f103 nucleo-64 board. for interfacing with st4sim.

 

 

    This topic has been closed for replies.