2024-11-27 6:21 PM
Hello... could anyone advise how to reduce the categories table on the left? i couldn't reduce it ! cos i couldn't see the pull-down menu "access only + MPU..." I m already using a 32" monitor!
2024-11-28 6:29 AM
Hello @HMSEdinburge
Actually, you can extend the Tab configuration to better display the parameter settings
Thx,
Souhaib
2024-11-28 6:44 AM
Yes, i already extended it to the end... only if you can advise how to reduce the categories menu.... mine is fixed dead unable to reduce it at all.
2024-11-28 8:17 AM
Are you using the last version of the CubeMX (V6.13.0). If no, please try using this version. From my side I can reduce the categories menu.
2024-11-28 4:09 PM
i m using STM32CubeIDE v1.15.1 no CubeMX...or how to check cubemx?
2024-11-28 4:25 PM
ok i see, i m using Cubemx 6.12.1.202409122..
2024-11-28 4:30 PM
how to upgrade to CubeMX (V6.13.0).
2024-11-29 1:18 AM
Hello
If you are using CubeMX standalone you can upgrade by clicking on Help>Check for update, then new STM32CubeMX Release as below:
The same way in STM32CubeIDE, you can find updates in Help > Check for updates.
Thx.