2022-12-22 10:26 AM
Hi
I trace (or I try) uint32 variable (counter increased by the HOST USB interrupt) to trace MSC class problems (BTW many bugs in HAL USB Host library). I receive about 2 million traces in about 80 seconds. The problem is that eclipse if freezing and cannot be recovered from that state. Do you know any solution (perhaps another SWV free trace software?)
2022-12-23 01:21 AM
Hello pj_stm,
Thank you for sharing your problem !
In order to well understand your issue could you please provide which CubeIDE version and the MCU you are using.
Regards,
Rim
2022-12-23 03:26 AM
Hi @Rim LANDOLSI
STM32CubeIDE
Version: 1.11.0
Build: 13638_20221122_1308 (UTC)
OS: Windows 10, v.10.0, x86_64 / win32
Java vendor: Eclipse Adoptium
Java runtime version: 11.0.16+8
Java version: 11.0.16
From Sytem info:
Processor Intel(R) Core(TM) i9-9980HK CPU @ 2.40GHz, 2400 Mhz, 8 Core(s), 16 Logical Processor(s)
Installed Physical Memory (RAM) 64.0 GB
2022-12-27 03:22 AM
Hello pj_stm ,
I have checked from my side but I cannot reproduce the same behavior you encountered. For that could you please provide the project where your issue occurs to help us reproduce this behavior and further analyze the interrupt and the changes you have made.
Thanks,
Rim