2024-01-17 9:17 AM
hello,
I have the same problem posted by H.Ahmed on October 2022, read also in other posts:
"Failed to start GDB Server Error Initializing ST-LINK device
Reason (18) Could not verify ST device!"
I tried all suggestions found on web, but no help.
I'm using STM32CubeIde 1.14.1, ST-Link V2 (updated)
Connection is very simple and should be OK, because if i program the device wth ST-Link Utility
or with STM32CubeProgrammer, all works fine.
I tried with CubeIde 1.8.0 as suggested in another post, but no luck.
Even older projects who i made some years ago, now have the same problem.
I read also on a post that someone from ST apologizes for this problem who is an older
bug reappeared now.
Hope there is a solution, because it would be very frustrating if i'm constrained
to change an IDE who i love, and if i'm unable to mantain older projects.
Thanks in advance
elvisee
Solved! Go to Solution.
2024-01-18 2:58 PM - edited 2024-01-18 2:59 PM
Hello @Mauri
To have the most probable device marking for each product. Check the product Package then refer to the TN1433 for verification.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-18 11:45 PM
>Is the difference the ST LOGO on the bottom?
Would you buy a Porsche , but no Porsche logo anywhere on the car ??
So, yes, no logo = anybody building this and "promising", some XXxxx chip is inside. Maybe ok - or not.
But even with some logo, still could be a copy . To know for 100% its genuine, buy direct from manufacturer (or its distributors) or do a test procedure with the chip, that proves its exactly what is written on it.
2024-01-19 6:52 AM
The best way to get a genuine part is via a reputable distributor.
Not to mention you're unlikely to get a genuine part on a counterfeit programmer, regardless of marking, as reputable distributors don't sell knockoff boards.