2023-10-06 01:22 PM
After having a problem with the generic Linux installation I uninstalled STM32CubeIDE and instead installed the Debian version. It loads up but when I click on File>New STM32 Project it says STM32 target or STM32CubeIDE example selection is required. Can't progress past that point. Log file attached
2023-10-19 06:40 AM - edited 2023-10-19 06:41 AM
Hello @Dabbo,
Thank you for posting.
Can you share the .log file and provide a screenshot of the STM32CubeIDE issue.
Thanks.
Mahmoud.