cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE crashing on startup Ubuntu

Dabbo
Associate III

After having a problem with the generic Linux installation I uninstalled STM32CubeIDE and instead installed the Debian version. It loads up but when I click on File>New STM32 Project it says STM32 target or STM32CubeIDE example selection is required. Can't progress past that point. Log file attached

 

 

1 REPLY 1
Mahmoud Ben Romdhane
ST Employee

Hello @Dabbo,

Thank you for posting.

Can you share the .log file and provide a screenshot of the STM32CubeIDE issue.

Thanks.

Mahmoud.