cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.14.0 -> old issue

padawan
Senior

Hello

the brand new 1.14.0 has the same issue like the older one.

padawan_0-1700729625642.png

an unnecessary file is opened after the 2nd debug session.

It's annoying that STM can't get this solved.

padawan

 

9 REPLIES 9
Souhaib MAZHOUD
ST Employee

Hello @padawan 

First let me thank you for posting!

In order to optimize the debugging session and stop opening the source file please follow the steps mentioned in this Thread.

Thank you.

Souhaib

Thanks for this,

i followed the thread but it will not work.

if i open the debug session it open the .s fille

padawan_0-1700732028425.png

padawan

 

Souhaib MAZHOUD
ST Employee

Hello @padawan 

Thanks for reporting.

Actually, after checking internally, this is a known issue that have been already reported to dev team and tracked with the internal ticket 162500 and this will be fixed asap.

Thx

Souhaib 

@Souhaib MAZHOUD Any chance you can give us some feedback on the progress of internal ticket 162500

3 months passed. but sadly still didn't fixed...

Peter-M2PRO
Associate

Almost 4 years of jumping to random files after pressing the Run button. What's another 4 months...

@Souhaib,

Opening an internal ticket is not a solution, it is poor.
An "asap" that takes 4 years is certainly not a solution.

padawan

 

Gproka
Associate

Same issue, version: Version: 1.15.1,  Win11, new CubeIDE installation. Problem started at the very first project (I started to learn programming MCUs recently) . 

After 4 years is still not resolved...

 

What is the status? Can you please provide an update and an ETA?

 

Thank you :)