cancel
Showing results for 
Search instead for 
Did you mean: 

ST link error: Failed to bind to port 61235; Failure starting SWV server

meena
Associate III

Hi I am experiencing an issue on my IDE I couldn't able to Run/Debug .However the ST Link can be communicated with the target in STM32 Cube programmer but not in STM32 cube IDE.

meena_0-1742378983077.png

Console  Error:

STMicroelectronics ST-LINK GDB server. Version 7.7.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Failed to bind to port 61235, error code -1: No error

Failure starting SWV server on TCP port: 61235

Failed to bind to port 61234, error code -1: No error

Failure starting GDB server: TCP port 61234 not available.

Shutting down...

Exit.

 

 

Can someone Please help me

 

1 ACCEPTED SOLUTION

Accepted Solutions

@meena wrote:

Failed to bind to port 61235, error code -1: No error

Failure starting SWV server on TCP port: 61235


Suggest a "network" issue (even if everything is local to the same PC).

STM32CubeIDE does require some Windows Firewall exceptions - presumably for this kind of stuff.

So maybe something has messed with that...?

View solution in original post

13 REPLIES 13

Please post a legible screenshot.

mÆŽALLEm
ST Employee

Hello @meena ,

The image shared is not clear. So please share a better picture resolution.

Also you didn't mention which product? which board are you using? ST board? custom board? 

Are you using an external ST-LINK? if yes, is it a genuine ST-LINK?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

 

meena_2-1742380627692.png

I am using STM32 Discovery Kit  board to program my prototype.My target have STM32G030K8 MCU. I can program hex file with STM32 Cube Programmer but not able to use STM32Cube IDE for debugging 


@mÆŽALLEm wrote:

Are you using an external ST-LINK? if yes, is it a genuine ST-LINK?


@meena see: 

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/ta-p/49471

in particular:

https://community.st.com/t5/stm32-mcus/how-to-recognize-a-genuine-st-link-v2-versus-a-cloned-one/tac-p/703663/highlight/true#M965

 


@mÆŽALLEm wrote:

Also you didn't mention which product? which board are you using? ST board? custom board? 


@meena The article How to write your question to maximize your chances to find a solution will help you with the information to provide, and other tips ...

I am using STM 32 Discovery Kit as my ST link it worked fine all of a sudden I am experiencing this error.


@meena wrote:

I am using STM 32 Discovery Kit as my ST link it worked fine all of a sudden I am experiencing this error.


Which Discovery board? please provide the exact board name.

"as my ST link it worked fine"

-> Which ST-LINK? could you please provide a photo?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

WhatsApp Image 2025-03-19 at 11.41.02.jpeg

 

 

This is the board usually I use for my development and debugging STM32F407G-DISC1 .I am finding issues on working in STM CUBE IDE.I can talk to the target withSTM 32Cube Programmer.I am confused why this happening.Please help

Why is the board still in its plastic packaging??!

 


@meena wrote:

This is the board usually I use for my development and debugging STM32F407G-DISC1 


So you're using the ST-Link on the Discovery board to program/debug a custom board?
Does the ST-Link work OK for debugging the Discovery board itself?

As you have succeded with CubeProgrammer but not with CubeIDE. It could be something related to the debug config in CubeIDE.

This is from a STM32F4 project:

mALLEm_0-1742389827049.png

Try to check "ST-LINK S/N" check box and click on "scan" button, do you get the serial number of the ST-LINK?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.