2024-09-28 6:22 PM
I am using Microsoft Surface Laptop with ARM processor.
Laptop I am using is - Microsoft Surface Pro 13" with Snapdragon X Plus (10 Core) processor.
I have installed STM32 CubeIDE and it does install. But while I try to upload code, it fails saying -
"No ST-link Detected"
I can also see that drivers are not installed on device manager. I really do need to work and test on things on the go. I am sure there is a way to work around this. Looking forward to help. Thanks.
2024-09-29 2:05 AM
What is your ST-Link: standalone like ST-Link v3 MINIE or on-board?
Does Device Manager show anything at all for it?
2024-10-08 8:18 AM
Hi,
I have a Nucleo-F411RE board. I do so driver fail at detecting device.
I downloaded the driver 'en.stsw-link009' but I see it only has x86 and AMD64 titled folders in it. Didn't see anything for ARM.
Your advice is appreciated.
2024-10-08 8:25 AM
I don't believe ARM is a supported platform currently, not sure where it is on the roadmap.
>>I really do need to work and test on things on the go.
I'd imagine one could find sub $200 x86-64 laptops/desktops if it's mission critical..