2019-07-02 10:45 AM
Hi.
When I use -JTAGConf option like this
I get this
What should I do?
Thanks
STM32CubeIDE
Version: 1.0.0
Build: 2872_20190423-2022 (UTC)
2019-07-02 01:04 PM
Perhaps try with 1.01 rather than try to re-litigate failures in old versions.
2019-07-02 01:07 PM
If still failing in 1.01 flag to @Markus GIRDLAND
2019-07-02 02:42 PM
Ok, thanks. But it still does not work. @Markus GIRDLAND
STM32CubeIDE
Version: 1.0.1
Build: 3139_20190612-1256 (UTC)
2019-07-03 07:33 AM
Looking into this at the moment, will let you know once I know more.
2019-07-04 12:54 AM
I could use some additional information.
Could you try to start the Segger J-Link GDB Server manually with the option bytes required? And then post the results?
2019-07-04 03:32 AM
Yes, what should I do?
2020-02-05 05:03 AM
Same problem here but different version.
CubeIde 1.2.0
JLinkARM.dll V6.62a
2020-07-16 02:05 AM
Problem still present in CubeIDE 1.3.1
Has anybody found a workarround?
2020-09-18 12:54 AM
Hello, I have the same problem, even in the CUbeide release 1.4.2.
Regards