cancel
Showing results for 
Search instead for 
Did you mean: 

SEGGER J-Link, -JTAGConf option fail

APhoe
Associate II

Hi.

When I use -JTAGConf option like this0690X000009YKHpQAO.png

I get this

0690X000009YKIOQA4.png

What should I do?

Thanks

STM32CubeIDE

Version: 1.0.0

Build: 2872_20190423-2022 (UTC)

10 REPLIES 10

Perhaps try with 1.01 rather than try to re-litigate failures in old versions.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

If still failing in 1.01 flag to @Markus GIRDLAND​ 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Ok, thanks. But it still does not work. @Markus GIRDLAND​ 

STM32CubeIDE

Version: 1.0.1

Build: 3139_20190612-1256 (UTC)

Looking into this at the moment, will let you know once I know more.

I could use some additional information.

Could you try to start the Segger J-Link GDB Server manually with the option bytes required? And then post the results?

Yes, what should I do?​

Ba5tian
Associate II

Same problem here but different version.

CubeIde 1.2.0

JLinkARM.dll V6.62a

MKell.1
Associate

Problem still present in CubeIDE 1.3.1

Has anybody found a workarround?

DVicc.1
Associate II

Hello, I have the same problem, even in the CUbeide release 1.4.2.

Regards