2024-09-17 12:01 AM
2024-09-17 12:15 PM
this started happening to me after installing a Copilot plugin from Eclipse marketplace.
Uninstalling the plugin didn't help.
I reinstalled eclipse and this fixed the problem.
2024-09-17 11:11 PM - edited 2024-09-17 11:32 PM
hi,
was it this one? https://marketplace.eclipse.org/content/copilot4eclipse
i have the same problem, also installed this plugin and it happened all of a sudden. for some time it did work. i did not change anything and *poff* i got this error
i have the same error in another eclipse based IDE (where i also installed this plugin)
in the beginning it worked flawlessly
2024-09-17 11:29 PM
Ok, I had also installed the Copilot plugin. At the beginning everything worked and then yesterday suddenly this error message when searching.
Now I have reinstalled the CubeIde, but still without Copilot Plugin, at the moment the search function works again.
2024-09-25 6:05 AM
Hello
Thanks for posting :).
The copilot plugin for Eclipse is not compatible with the Eclipse CDT version on which STM32CubeIDE is based.
The investigation is ongoing internally and it should be fixed when the Eclipse version used by STM32CubeIDE is upgraded. This will be included in future releases.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-25 6:08 AM
hi,
there was an update from Genuitec. This posting explains the details. With this version it should be fixed
https://github.com/Genuitec/Copilot4Eclipse-community/discussions/23